<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to control the Builtin LED Light of Teensy 3.5 using uTasker? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-control-the-Builtin-LED-Light-of-Teensy-3-5-using-uTasker/m-p/732955#M44817</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alres&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LED is 'attached' to the watchdog retrigger. It is called each time the retrigger takes place via the macro&lt;BR /&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;TOGGLE_WATCHDOG_LED()&lt;/STRONG&gt;&lt;BR /&gt;which is defined as&lt;BR /&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;#define TOGGLE_WATCHDOG_LED()&amp;nbsp; _TOGGLE_PORT(C, BLINK_LED)&lt;/STRONG&gt;&lt;BR /&gt;for the Teensy 3.5 (see &lt;EM&gt;app_hw_kinetis.h&lt;/EM&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you wanted to have no LED, for example, you could just make the macro dummy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;#define TOGGLE_WATCHDOG_LED()&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The watchdog retrigger rate is set in the watchdog task's properties in &lt;EM&gt;TaskConfig.h&lt;/EM&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;{"Wdog",&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnTaskWatchdog, NO_QUEUE,&amp;nbsp;&amp;nbsp; 0, (DELAY_LIMIT)(0.2 * SEC),&amp;nbsp; UTASKER_GO}, // watchdog task (runs immediately and then periodically)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here you see that it is set at 2.5Hz (200ms retrigger rate) as standard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can change this time to make it faster or slower, but remember that you will be changing also the watchdog retrigger rate, which you need to have at least at a periodic rate less that the watchog's timeout (with a little margin)!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A simply way to make it slower without changing the watchdog retrigger rate is to use something like&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;#define TOGGLE_WATCHDOG_LED()&amp;nbsp; if (++(my_variable &amp;gt;= 2)) {my_variable = 0; _TOGGLE_PORT(C, BLINK_LED);}&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will need to add &lt;EM&gt;my_variable&lt;/EM&gt; defined globally and the &amp;gt;= 2 will halve the rate that the LED is toggled at, &amp;gt;= 3 would divide by 3 etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Note that the LED is used generally as a "heart-beat" indication. It allows you to simply see that the board is actually operating and, as long as it flashes at a constant and smooth rate, that the whole system is running stably. If it were to freeze or become jittery it shows that there is either an error (eg. a hard fault or endless loop, which will cause a watchdog reset after a short delay) or that there is some processing that is causing the watchdog task to be delayed.&lt;BR /&gt;The watchdog task itself is there to detect such issues - it is executed periodically as long as everything is operating normally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Personally I hate demonstration projects that don't actually show that they are alive simply by looking at the board, as I hate demonstration projects that don't incorporate a watchdog concept as standard....even in a most primitive "blinky" configuration....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jan 2018 16:37:49 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2018-01-17T16:37:49Z</dc:date>
    <item>
      <title>How to control the Builtin LED Light of Teensy 3.5 using uTasker?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-control-the-Builtin-LED-Light-of-Teensy-3-5-using-uTasker/m-p/732954#M44816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to control the Builtin LED Light of Teensy 3.5 using uTasker?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because the rate of the flashing of led light is fast. How can i control it ? Please Help :smileysad:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 15:26:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-control-the-Builtin-LED-Light-of-Teensy-3-5-using-uTasker/m-p/732954#M44816</guid>
      <dc:creator>alresarena</dc:creator>
      <dc:date>2018-01-17T15:26:58Z</dc:date>
    </item>
    <item>
      <title>Re: How to control the Builtin LED Light of Teensy 3.5 using uTasker?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-control-the-Builtin-LED-Light-of-Teensy-3-5-using-uTasker/m-p/732955#M44817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alres&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LED is 'attached' to the watchdog retrigger. It is called each time the retrigger takes place via the macro&lt;BR /&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;TOGGLE_WATCHDOG_LED()&lt;/STRONG&gt;&lt;BR /&gt;which is defined as&lt;BR /&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;#define TOGGLE_WATCHDOG_LED()&amp;nbsp; _TOGGLE_PORT(C, BLINK_LED)&lt;/STRONG&gt;&lt;BR /&gt;for the Teensy 3.5 (see &lt;EM&gt;app_hw_kinetis.h&lt;/EM&gt;)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you wanted to have no LED, for example, you could just make the macro dummy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;#define TOGGLE_WATCHDOG_LED()&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The watchdog retrigger rate is set in the watchdog task's properties in &lt;EM&gt;TaskConfig.h&lt;/EM&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;{"Wdog",&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fnTaskWatchdog, NO_QUEUE,&amp;nbsp;&amp;nbsp; 0, (DELAY_LIMIT)(0.2 * SEC),&amp;nbsp; UTASKER_GO}, // watchdog task (runs immediately and then periodically)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here you see that it is set at 2.5Hz (200ms retrigger rate) as standard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can change this time to make it faster or slower, but remember that you will be changing also the watchdog retrigger rate, which you need to have at least at a periodic rate less that the watchog's timeout (with a little margin)!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A simply way to make it slower without changing the watchdog retrigger rate is to use something like&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="font-family: courier new, courier, monospace;"&gt;#define TOGGLE_WATCHDOG_LED()&amp;nbsp; if (++(my_variable &amp;gt;= 2)) {my_variable = 0; _TOGGLE_PORT(C, BLINK_LED);}&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will need to add &lt;EM&gt;my_variable&lt;/EM&gt; defined globally and the &amp;gt;= 2 will halve the rate that the LED is toggled at, &amp;gt;= 3 would divide by 3 etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Note that the LED is used generally as a "heart-beat" indication. It allows you to simply see that the board is actually operating and, as long as it flashes at a constant and smooth rate, that the whole system is running stably. If it were to freeze or become jittery it shows that there is either an error (eg. a hard fault or endless loop, which will cause a watchdog reset after a short delay) or that there is some processing that is causing the watchdog task to be delayed.&lt;BR /&gt;The watchdog task itself is there to detect such issues - it is executed periodically as long as everything is operating normally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Personally I hate demonstration projects that don't actually show that they are alive simply by looking at the board, as I hate demonstration projects that don't incorporate a watchdog concept as standard....even in a most primitive "blinky" configuration....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 16:37:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-control-the-Builtin-LED-Light-of-Teensy-3-5-using-uTasker/m-p/732955#M44817</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-01-17T16:37:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to control the Builtin LED Light of Teensy 3.5 using uTasker?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-control-the-Builtin-LED-Light-of-Teensy-3-5-using-uTasker/m-p/732956#M44818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you so much for the advise Sir Mark :smileyhappy:&amp;nbsp; I'll try this :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jan 2018 22:24:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-control-the-Builtin-LED-Light-of-Teensy-3-5-using-uTasker/m-p/732956#M44818</guid>
      <dc:creator>alresarena</dc:creator>
      <dc:date>2018-01-18T22:24:33Z</dc:date>
    </item>
  </channel>
</rss>