<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K81 blhost spi error</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-blhost-spi-error/m-p/732928#M44814</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on the K81. I am using blhost with spi (run mode with 4Mbps) to write .sb file to the QSPI memory. But I am getting following error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Inject command 'receive-sb-file'&lt;BR /&gt;Preparing to send 345760 (0x546a0) bytes to the target.&lt;BR /&gt;Successful generic response to command 'receive-sb-file'&lt;BR /&gt;(1/1)0%Error: read_start_byte() timeout after 10.037 seconds&lt;BR /&gt;Data phase write aborted by status 0x5 kStatus_Timeout&lt;BR /&gt;Error: read_start_byte() timeout after 10.025 seconds&lt;BR /&gt;Response status = 10004 (0x2714) No response packet from target device.&lt;BR /&gt;Wrote 672 of 345760 bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please help me with this.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Feb 2018 10:23:32 GMT</pubDate>
    <dc:creator>kaustubhkulkarn</dc:creator>
    <dc:date>2018-02-09T10:23:32Z</dc:date>
    <item>
      <title>K81 blhost spi error</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-blhost-spi-error/m-p/732928#M44814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on the K81. I am using blhost with spi (run mode with 4Mbps) to write .sb file to the QSPI memory. But I am getting following error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Inject command 'receive-sb-file'&lt;BR /&gt;Preparing to send 345760 (0x546a0) bytes to the target.&lt;BR /&gt;Successful generic response to command 'receive-sb-file'&lt;BR /&gt;(1/1)0%Error: read_start_byte() timeout after 10.037 seconds&lt;BR /&gt;Data phase write aborted by status 0x5 kStatus_Timeout&lt;BR /&gt;Error: read_start_byte() timeout after 10.025 seconds&lt;BR /&gt;Response status = 10004 (0x2714) No response packet from target device.&lt;BR /&gt;Wrote 672 of 345760 bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please help me with this.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 10:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-blhost-spi-error/m-p/732928#M44814</guid>
      <dc:creator>kaustubhkulkarn</dc:creator>
      <dc:date>2018-02-09T10:23:32Z</dc:date>
    </item>
    <item>
      <title>Re: K81 blhost spi error</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-blhost-spi-error/m-p/732929#M44815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm not sure if you connect your system correctly. Please review &amp;lt;Kinetis blhost User's Guide.pdf&amp;gt; for detail. In Appendix C, it describes how to download code by blhost if you want to use SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 09:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-blhost-spi-error/m-p/732929#M44815</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-02-13T09:33:01Z</dc:date>
    </item>
  </channel>
</rss>