<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 When exactly is PIT reset? Kinetis</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-exactly-is-PIT-reset-Kinetis/m-p/225914#M4470</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is a Periodic Interrupt Timer (PIT) reset the moment the rollover/interrupt occurs, or the moment the interrupt flag is cleared?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if poor code was involved and the interrupt took way to long, would such and interrupt routine be re-entrant? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Nov 2013 17:33:06 GMT</pubDate>
    <dc:creator>ignisuti</dc:creator>
    <dc:date>2013-11-25T17:33:06Z</dc:date>
    <item>
      <title>When exactly is PIT reset? Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-exactly-is-PIT-reset-Kinetis/m-p/225914#M4470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is a Periodic Interrupt Timer (PIT) reset the moment the rollover/interrupt occurs, or the moment the interrupt flag is cleared?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, if poor code was involved and the interrupt took way to long, would such and interrupt routine be re-entrant? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2013 17:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-exactly-is-PIT-reset-Kinetis/m-p/225914#M4470</guid>
      <dc:creator>ignisuti</dc:creator>
      <dc:date>2013-11-25T17:33:06Z</dc:date>
    </item>
    <item>
      <title>Re: When exactly is PIT reset? Kinetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-exactly-is-PIT-reset-Kinetis/m-p/225915#M4471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Joe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, PIT load their start values, as specified in their LDVAL registers, then count down until they reach 0. Each time a timer reaches 0, it will generate a trigger pulse and set the interrupt flag. Then they load their respective start value again. So it can reset value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope my reply can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2013 00:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/When-exactly-is-PIT-reset-Kinetis/m-p/225915#M4471</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2013-11-26T00:58:53Z</dc:date>
    </item>
  </channel>
</rss>