<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 JTAG Signals on K66F</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-Signals-on-K66F/m-p/728360#M44544</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using K66F for our controller and have the following questions:&lt;/P&gt;&lt;P&gt;PTA0~~PTA4 is used as JTAG to program MCU by PE tool and it works fine in our controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I re-use these signals for other purpose, like UART0 or FTM, and etc? It can be re-configured after programming?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Feb 2018 21:09:10 GMT</pubDate>
    <dc:creator>a8Chcx</dc:creator>
    <dc:date>2018-02-07T21:09:10Z</dc:date>
    <item>
      <title>JTAG Signals on K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-Signals-on-K66F/m-p/728360#M44544</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using K66F for our controller and have the following questions:&lt;/P&gt;&lt;P&gt;PTA0~~PTA4 is used as JTAG to program MCU by PE tool and it works fine in our controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I re-use these signals for other purpose, like UART0 or FTM, and etc? It can be re-configured after programming?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Feb 2018 21:09:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-Signals-on-K66F/m-p/728360#M44544</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2018-02-07T21:09:10Z</dc:date>
    </item>
    <item>
      <title>Re: JTAG Signals on K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-Signals-on-K66F/m-p/728361#M44545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes. But not recommend.&lt;BR /&gt;You may meet some problem next time you want to flash it. See:&lt;A href="https://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-low-power/"&gt;Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to disable the EzPort and NMI function on PTA0~PTA4, please read "Table 7-3. Flash Option Register Bit Definitions" in &lt;A href="https://www.nxp.com/docs/en/reference-manual/K66P144M180SF5RMV2.pdf"&gt;K66P144M180SF5RMV2&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7008i07B488B25087C6F2/image-size/large?v=v2&amp;amp;px=999" title="Table 7-3. Flash Option Register Bit Definitions.PNG" alt="Table 7-3. Flash Option Register Bit Definitions.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Feb 2018 08:54:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/JTAG-Signals-on-K66F/m-p/728361#M44545</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-02-11T08:54:55Z</dc:date>
    </item>
  </channel>
</rss>