<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Failed to resume target process., ARM GDI Protocol Adapter : An error occurred while trying to write memory. The Debugger can not write memory. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failed-to-resume-target-process-ARM-GDI-Protocol-Adapter-An/m-p/225626#M4438</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm creating a new project 'deleteme' as a Bareboard project for my KL15Z128 design... I cannot seem to debug, I haven't touched the project initial code...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The funny thing is my CW 10.4 was working great just 3 weeks ago with my prototype, now it doesn't since I connect my prototype that worked ok with mi CW 10.4 and now it doesn't work!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't touched the project since the last time it worked 3 weeks ago... did something expired in my CW instalation, or did it automatically update to something that doesn't work now???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following the complete output of the J-Link trace:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Executing Initialization File: C:\Users\Carlos\workspace\deleteme1/Project_Settings/Debugger/init_kinetis.tcl&lt;/P&gt;&lt;P&gt;radix x &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config hexprefix 0x &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemIdentifier p &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemWidth 32 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemAccess 32 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemSwap off &lt;/P&gt;&lt;P&gt;cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF &lt;/P&gt;&lt;P&gt;failed on register write: LR &lt;/P&gt;&lt;P&gt;cmdwin::reg Breakpoint Unit Registers/BP_COMP0 = 0x0 &lt;/P&gt;&lt;P&gt;failed on register write: BP_COMP0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Breakpoint Unit Registers/BP_COMP1 = 0x0 &lt;/P&gt;&lt;P&gt;failed on register write: BP_COMP1 &lt;/P&gt;&lt;P&gt;cmdwin::reg Core Debug Registers/DEMCR = 0x1000001 &lt;/P&gt;&lt;P&gt;failed on register write: DEMCR &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0 &lt;/P&gt;&lt;P&gt;failed on register write: DWT_FUNCTION0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0 &lt;/P&gt;&lt;P&gt;failed on register write: DWT_FUNCTION1 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please Help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Oct 2013 08:11:01 GMT</pubDate>
    <dc:creator>lokuate</dc:creator>
    <dc:date>2013-10-23T08:11:01Z</dc:date>
    <item>
      <title>Failed to resume target process., ARM GDI Protocol Adapter : An error occurred while trying to write memory. The Debugger can not write memory.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failed-to-resume-target-process-ARM-GDI-Protocol-Adapter-An/m-p/225626#M4438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm creating a new project 'deleteme' as a Bareboard project for my KL15Z128 design... I cannot seem to debug, I haven't touched the project initial code...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The funny thing is my CW 10.4 was working great just 3 weeks ago with my prototype, now it doesn't since I connect my prototype that worked ok with mi CW 10.4 and now it doesn't work!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I haven't touched the project since the last time it worked 3 weeks ago... did something expired in my CW instalation, or did it automatically update to something that doesn't work now???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following the complete output of the J-Link trace:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Executing Initialization File: C:\Users\Carlos\workspace\deleteme1/Project_Settings/Debugger/init_kinetis.tcl&lt;/P&gt;&lt;P&gt;radix x &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config hexprefix 0x &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemIdentifier p &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemWidth 32 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemAccess 32 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemSwap off &lt;/P&gt;&lt;P&gt;cmdwin::reg User\/System Mode Registers/LR = 0xFFFFFFFF &lt;/P&gt;&lt;P&gt;failed on register write: LR &lt;/P&gt;&lt;P&gt;cmdwin::reg Breakpoint Unit Registers/BP_COMP0 = 0x0 &lt;/P&gt;&lt;P&gt;failed on register write: BP_COMP0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Breakpoint Unit Registers/BP_COMP1 = 0x0 &lt;/P&gt;&lt;P&gt;failed on register write: BP_COMP1 &lt;/P&gt;&lt;P&gt;cmdwin::reg Core Debug Registers/DEMCR = 0x1000001 &lt;/P&gt;&lt;P&gt;failed on register write: DEMCR &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION0 = 0x0 &lt;/P&gt;&lt;P&gt;failed on register write: DWT_FUNCTION0 &lt;/P&gt;&lt;P&gt;cmdwin::reg Data Watchpoint and Trace Unit Registers/DWT_FUNCTION1 = 0x0 &lt;/P&gt;&lt;P&gt;failed on register write: DWT_FUNCTION1 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please Help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Oct 2013 08:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failed-to-resume-target-process-ARM-GDI-Protocol-Adapter-An/m-p/225626#M4438</guid>
      <dc:creator>lokuate</dc:creator>
      <dc:date>2013-10-23T08:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process., ARM GDI Protocol Adapter : An error occurred while trying to write memory. The Debugger can not write memory.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failed-to-resume-target-process-ARM-GDI-Protocol-Adapter-An/m-p/225627#M4439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi carlos,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Try making a new workspace for the same project and check that power supply to the board is proper.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nasreen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2013 04:54:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failed-to-resume-target-process-ARM-GDI-Protocol-Adapter-An/m-p/225627#M4439</guid>
      <dc:creator>nasreenshaikh</dc:creator>
      <dc:date>2013-10-24T04:54:11Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process., ARM GDI Protocol Adapter : An error occurred while trying to write memory. The Debugger can not write memory.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failed-to-resume-target-process-ARM-GDI-Protocol-Adapter-An/m-p/225628#M4440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Really i found the same problem:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ARM GDI Protocol Adapter : An error occurred while trying to write memory. The Debugger can not write memory.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something happened with hardware connection. I tried several projects but same problem all time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To solve this problem i put device in the forced reset by button and in time of reset i start debugging. The CW started debugging and after some delay i switch off my reset button to start the controller.&lt;/P&gt;&lt;P&gt;Everything become good.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Nov 2013 13:39:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Failed-to-resume-target-process-ARM-GDI-Protocol-Adapter-An/m-p/225628#M4440</guid>
      <dc:creator>alexandergutor</dc:creator>
      <dc:date>2013-11-23T13:39:56Z</dc:date>
    </item>
  </channel>
</rss>