<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KEA128 MSCAN</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-MSCAN/m-p/725212#M44375</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Hi Sharad Mehta,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; This is the same question as your another post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/467867"&gt;KEA128 MSCAN&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check that post, I have answered you.&lt;/P&gt;&lt;P&gt;&amp;nbsp; You can use the CW project, or you create the KEIL KEA project, then add the CW CAN driver to your keil project, it also works.&lt;/P&gt;&lt;P&gt;&amp;nbsp; After you create the keil project, and add the MSCAN driver have problems, please let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jan 2018 03:09:22 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2018-01-16T03:09:22Z</dc:date>
    <item>
      <title>KEA128 MSCAN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-MSCAN/m-p/725211#M44374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Need Keil example code/project to read and write CAN Messages.&lt;/P&gt;&lt;P&gt;Board TRK-KEA128&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 18:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-MSCAN/m-p/725211#M44374</guid>
      <dc:creator>sharadmehta</dc:creator>
      <dc:date>2018-01-15T18:20:28Z</dc:date>
    </item>
    <item>
      <title>Re: KEA128 MSCAN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-MSCAN/m-p/725212#M44375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Hi Sharad Mehta,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; This is the same question as your another post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/467867"&gt;KEA128 MSCAN&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check that post, I have answered you.&lt;/P&gt;&lt;P&gt;&amp;nbsp; You can use the CW project, or you create the KEIL KEA project, then add the CW CAN driver to your keil project, it also works.&lt;/P&gt;&lt;P&gt;&amp;nbsp; After you create the keil project, and add the MSCAN driver have problems, please let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 03:09:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-MSCAN/m-p/725212#M44375</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-01-16T03:09:22Z</dc:date>
    </item>
  </channel>
</rss>