<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK64F - RX buffer size is zero</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-RX-buffer-size-is-zero/m-p/724291#M44333</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using K64F with KSDK-1.4.0 and the supplied RTX(ARM).&lt;BR /&gt;This is a custom PCB and has an ethernet/PHY interface.&lt;BR /&gt;The ethernet is also working, the TCP/IP stack being used is the MDK-ARM Middleware(ARM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After a while by applying this PCB to the UDP storm tool (self-made), the Rx descriptor&lt;BR /&gt;information has an abnormal value after the Rx interrupt has occurred.&lt;BR /&gt;Specifically, it has the following information and the data length is 0.&lt;/P&gt;&lt;P&gt;----&lt;/P&gt;&lt;P&gt;Enhanced uDMA receive buffer descriptor(RxBD) infomation&lt;BR /&gt;&amp;nbsp;Data Length(Offset+0 Filed 15-0) =&amp;gt; 0x0000&lt;BR /&gt;&amp;nbsp;E(Offset+2 Field 15) =&amp;gt; 0&lt;/P&gt;&lt;P&gt;----&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know the exact reason to this.&lt;BR /&gt;Have you got any idea what shall I do? How can I recover from this error successfully?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, regards,&lt;BR /&gt;Katsuyuki Sasajima&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Mar 2018 06:50:55 GMT</pubDate>
    <dc:creator>katsuyukisasaji</dc:creator>
    <dc:date>2018-03-22T06:50:55Z</dc:date>
    <item>
      <title>K64F - RX buffer size is zero</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-RX-buffer-size-is-zero/m-p/724291#M44333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using K64F with KSDK-1.4.0 and the supplied RTX(ARM).&lt;BR /&gt;This is a custom PCB and has an ethernet/PHY interface.&lt;BR /&gt;The ethernet is also working, the TCP/IP stack being used is the MDK-ARM Middleware(ARM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After a while by applying this PCB to the UDP storm tool (self-made), the Rx descriptor&lt;BR /&gt;information has an abnormal value after the Rx interrupt has occurred.&lt;BR /&gt;Specifically, it has the following information and the data length is 0.&lt;/P&gt;&lt;P&gt;----&lt;/P&gt;&lt;P&gt;Enhanced uDMA receive buffer descriptor(RxBD) infomation&lt;BR /&gt;&amp;nbsp;Data Length(Offset+0 Filed 15-0) =&amp;gt; 0x0000&lt;BR /&gt;&amp;nbsp;E(Offset+2 Field 15) =&amp;gt; 0&lt;/P&gt;&lt;P&gt;----&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know the exact reason to this.&lt;BR /&gt;Have you got any idea what shall I do? How can I recover from this error successfully?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, regards,&lt;BR /&gt;Katsuyuki Sasajima&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Mar 2018 06:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-RX-buffer-size-is-zero/m-p/724291#M44333</guid>
      <dc:creator>katsuyukisasaji</dc:creator>
      <dc:date>2018-03-22T06:50:55Z</dc:date>
    </item>
  </channel>
</rss>