<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K70 DDR Configuration Issue with TWR-K70</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-DDR-Configuration-Issue-with-TWR-K70/m-p/721990#M44234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K70 SIM_MCR register [DDRCFG] field using to control the DDR memory types and drive strength.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;The DDR_CR53-55 register [Reserved] bits field function is not visible to customer.&lt;/SPAN&gt;&lt;BR /&gt;I do a similar test with TWR-K70F120M board, the 0x84806018 ~ 0x8480601b memory range value was modified during code operation.&lt;BR /&gt;For I don't know the customer application, I couldn't check if customer mentioned DDR2 memory range (0x84806018 ~ 0x8480601b) with the incorrect value.&lt;BR /&gt;While, if I write the fixed value to those memory range, such as 0x5555AAAA. I will read the correct value from those DDR2 memory range.&lt;BR /&gt;I am using below code for K70 Tower board DDR2 controller initialization.&lt;BR /&gt;We recommend customer to use the&lt;A href="https://www.nxp.com/downloads/en/initialization-boot-device-driver-code-generation/KINETIS_K70_DDR_INIT.exe"&gt; [Kinetis® K70 DDR memory initialization tool(REV 1.11.1)] tool&lt;/A&gt;:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;void twr_ddr2_script_init(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Enable DDR controller clock */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SIM_SCGC3 |= SIM_SCGC3_DDR_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Enable DDR pads and set slew rate */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SIM_MCR |= 0xC4;&amp;nbsp;&amp;nbsp; // bits were left out of the manual so there isn't a macro right now&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_RCR |= DDR_RCR_RST_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;* (vuint32 *)(0x400Ae1ac) = 0x01030203;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR00 = 0x00000400;&amp;nbsp;&amp;nbsp;&amp;nbsp; // DDRCLS = 4 is reserved??&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR02 = 0x02000031;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR03 = 0x02020506;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR04 = 0x06090202;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR05 = 0x02020302;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR06 = 0x02904002;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR07 = 0x01000303;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR08 = 0x05030201;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR09 = 0x020000c8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR10 = 0x03003207;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR11 = 0x01000000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR12 = 0x04920031;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR13 = 0x00000005;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR14 = 0x00C80002;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR15 = 0x00000032; //&amp;nbsp; | DDR_CR15_SREF_MASK ;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR16 = 0x00000001;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR20 = 0x00030300;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR21 = 0x00040232;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR22 = 0x00000000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR23 = 0x00040302;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR25 = 0x0A010201;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR26 = 0x0101FFFF;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR27 = 0x01010101;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR28 = 0x00000003;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR29 = 0x00000000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR30 = 0x00000001;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR34 = 0x02020101;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR36 = 0x01010201;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR37 = 0x00000200;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR38 = 0x00200000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR39 = 0x01010020;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR40 = 0x00002000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR41 = 0x01010020;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR42 = 0x00002000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR43 = 0x01010020;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR44 = 0x00000000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR45 = 0x03030303;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR46 = 0x02006401;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR47 = 0x01020202;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR48 = 0x01010064;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR49 = 0x00020101;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR50 = 0x00000064;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR52 = 0x02000602;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR53 = 0x03c80000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR54 = 0x03c803c8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR55 = 0x03c803c8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR56 = 0x020303c8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR57 = 0x01010002;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;asm("NOP");&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR00 |= 0x00000001;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while ((DDR_CR30 &amp;amp; 0x400) != 0x400);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;MCM_CR |= MCM_CR_DDRSIZE(1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jan 2018 06:26:55 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2018-01-16T06:26:55Z</dc:date>
    <item>
      <title>K70 DDR Configuration Issue with TWR-K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-DDR-Configuration-Issue-with-TWR-K70/m-p/721989#M44233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;TABLE width="600"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD style="background: white; padding: 3.0pt 3.0pt 3.0pt 3.0pt;"&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;&lt;BR /&gt; Customer is having a sporadic issue with DDR that i have narrowed down to this line of code: &lt;BR /&gt; &lt;BR /&gt; while (u--) { &lt;BR /&gt; *p++ ^= uSeed; &lt;BR /&gt; uSeed += 0x01020304; &lt;BR /&gt; } &lt;BR /&gt; where p is a address in ddr. read/modify/write to ddr, a very bus intensive operation. &lt;BR /&gt; &lt;BR /&gt; The error is always at the block of 4 bytes starting at offset 0x850, (p starts at address 0x848057c8, so address 0x84806018-0x8480601b). &lt;BR /&gt; &lt;BR /&gt; Customer has tried two DDR configs, one based off K70MemCtrol and one that matches the code used by bare metal and MQX. &lt;BR /&gt; &lt;BR /&gt; SIM_MCR &amp;amp;= 0xFFFFFF00; SIM_MCR |= 0x000000c4; DDR_RCR |= DDR_RCR_RST_MASK; DDR_PAD_CTRL = 0x01030203; //micrium (and MQX) DDR_CR00 = 0x00000400; DDR_CR02 = 0x02000031; DDR_CR03 = 0x02020506; DDR_CR04 = 0x06090202; DDR_CR05 = 0x02020302; DDR_CR06 = 0x02904002; DDR_CR07 = 0x01000303; DDR_CR08 = 0x05030201; DDR_CR09 = 0x020000c8; DDR_CR10 = 0x03003207; DDR_CR11 = 0x01000000; DDR_CR12 = 0x04920031; DDR_CR13 = 0x00000005; DDR_CR14 = 0x00C80002; DDR_CR15 = 0x00000032; DDR_CR16 = 0x00000001; DDR_CR20 = 0x00030300; DDR_CR21 = 0x00040232; DDR_CR22 = 0x00000000; DDR_CR23 = 0x00040302; DDR_CR25 = 0x0A010201; DDR_CR26 = 0x0101FFFF; DDR_CR27 = 0x01010101; DDR_CR28 = 0x00000003; DDR_CR29 = 0x00000000; DDR_CR30 = 0x00000001; DDR_CR34 = 0x02020101; DDR_CR36 = 0x01010201; DDR_CR37 = 0x00000200; DDR_CR38 = 0x00200000; DDR_CR39 = 0x01010020; DDR_CR40 = 0x00002000; DDR_CR41 = 0x01010020; DDR_CR42 = 0x00002000; DDR_CR43 = 0x01010020; DDR_CR44 = 0x00000000; DDR_CR45 = 0x03030303; DDR_CR46 = 0x02006401; DDR_CR47 = 0x01020202; DDR_CR48 = 0x01010064; DDR_CR49 = 0x00020101; DDR_CR50 = 0x00000064; DDR_CR52 = 0x02000602; DDR_CR53 = 0x03c80000; DDR_CR54 = 0x03c803c8; DDR_CR55 = 0x03c803c8; DDR_CR56 = 0x020303c8; DDR_CR57 = 0x01010002; &lt;BR /&gt; &lt;BR /&gt; /* &lt;BR /&gt; //MemInitTool DDR_CR00 = 0x00000400; // DDRCLS, start DDR_CR02 = 0x02007530; // initaref, tinit DDR_CR03 = 0x02020707; // tccd, wrlat, latgate, latlin DDR_CR04 = 0x07090202; // trasmin, trc, trrd, tbint DDR_CR05 = 0x02020302; // tmrd, trtp, trp, twtr DDR_CR06 = 0x00290402; // intwbr, trasmax, tmod DDR_CR07 = 0x01010303; // ccapen, ap, tckesr, clkpw DDR_CR08 = 0x06030301; // tdal, twr, trasdi, tras DDR_CR09 = 0x020000c8; // bstlen, nocmd, tdll DDR_CR10 = 0x02000808; // trpab, tcpd, tfaw DDR_CR11 = 0x01000000; // trefen, arefmode, aref, regdimm DDR_CR12 = 0x048a001e; // tref, trfc DDR_CR13 = 0x00000005; // pd, trefint DDR_CR14 = 0x00c70002; // txsr, tpdex DDR_CR15 = 0x00000015; // puref, sref, txsnr DDR_CR16 = 0x00000001; // lpctrl, clkdly, qkref DDR_CR17 = 0; DDR_CR18 = 0; DDR_CR19 = 0; DDR_CR20 = 0x00030300; // cksrx, cksre, lpre DDR_CR21 = 0x24040232; // mr1dat0, mr0dat0 DDR_CR22 = 0; DDR_CR25 = 0x0a010201; // aprebit, colsiz, addpins, bnk8 DDR_CR26 = 0x0101ffff; // bnkspt, addcol, cmdage, agecnt DDR_CR27 = 0x00010101; // swpen, rwen, prien, plen DDR_CR28 = 0x00000001; // cmdlatr, bigend, reduc, csmap DDR_CR29=0; DDR_CR30 = 0x00000001; // intack, rsyncrf DDR_CR31 = 0; DDR_CR34 = 0x00000101; // odtwrcs, odtrdcs DDR_CR37 = 0x00000200; // w2wsame, w2rsame, r2wsame, r2rsame DDR_CR38 = 0x00200000; // p0wrcnt, pupcs, pdncs DDR_CR39 = 0x00000020; // wp0, rp0, p0rdcnt DDR_CR40 = 0x00002000; // p1wrcnt, p0typ DDR_CR41 = 0x01010020; // wp1, rp1, p1rdcnt DDR_CR42 = 0x00002000; // p2wrcnt, p1typ DDR_CR43 = 0x02020020; // wp2, rp2, p2rdcnt DDR_CR44 = 0; DDR_CR45 = 0x00070b0f; // p0pri3, p0pri2, p0pri1, p0pri0 DDR_CR46 = 0x0f004000; // p1pri0, p0prirlx, p0ord DDR_CR47 = 0x0100070b; // p1ord, p1pri3, p1pri2, p1pri1 DDR_CR48 = 0x0b0f0040; // p2pri1, p2pri0, p1prirlx DDR_CR49 = 0x00020007; // p2ord, p2pri3, p2pri2 DDR_CR50 = 0x00000040; // p2prirlx DDR_CR51 = 0; DDR_CR52 = 0x02000602; // rddtenbas, phyrdlat, phywrltbs DDR_CR53 = 0; DDR_CR54 = 0; DDR_CR55 = 0; DDR_CR56 = 0x02030000; // wrlatadj, rdlatadj DDR_CR57 = 0x01000000; // odtalten &lt;BR /&gt; */ asm("NOP"); DDR_CR00 |= 0x00000001; while ((DDR_CR30 &amp;amp; 0x400) != 0x400); MCM_CR |= MCM_CR_DDRSIZE(1); &lt;BR /&gt; &lt;BR /&gt; What is the difference in setting DDRCFG in SIM_MCR to half strenght and the other to full strength? Both are design for the same TWR-K70 board. &lt;BR /&gt; &lt;BR /&gt; The bare metal/MQX code version sets DDR_CR53-55 (among other), however this conflicts with the ref manual. It has those as 'RESERVED'. Where did the reserved values come from? &lt;BR /&gt; &lt;BR /&gt; Thank you in advance,&lt;BR /&gt; Scott&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: white; background: white;"&gt;Thread Id:&amp;nbsp;ref:_00D20NBgb._500571g5flJ:ref&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt; color: black; background: white;"&gt;------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 14:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-DDR-Configuration-Issue-with-TWR-K70/m-p/721989#M44233</guid>
      <dc:creator>ScottKerstein</dc:creator>
      <dc:date>2018-01-15T14:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: K70 DDR Configuration Issue with TWR-K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-DDR-Configuration-Issue-with-TWR-K70/m-p/721990#M44234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K70 SIM_MCR register [DDRCFG] field using to control the DDR memory types and drive strength.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;The DDR_CR53-55 register [Reserved] bits field function is not visible to customer.&lt;/SPAN&gt;&lt;BR /&gt;I do a similar test with TWR-K70F120M board, the 0x84806018 ~ 0x8480601b memory range value was modified during code operation.&lt;BR /&gt;For I don't know the customer application, I couldn't check if customer mentioned DDR2 memory range (0x84806018 ~ 0x8480601b) with the incorrect value.&lt;BR /&gt;While, if I write the fixed value to those memory range, such as 0x5555AAAA. I will read the correct value from those DDR2 memory range.&lt;BR /&gt;I am using below code for K70 Tower board DDR2 controller initialization.&lt;BR /&gt;We recommend customer to use the&lt;A href="https://www.nxp.com/downloads/en/initialization-boot-device-driver-code-generation/KINETIS_K70_DDR_INIT.exe"&gt; [Kinetis® K70 DDR memory initialization tool(REV 1.11.1)] tool&lt;/A&gt;:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;void twr_ddr2_script_init(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Enable DDR controller clock */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SIM_SCGC3 |= SIM_SCGC3_DDR_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;/* Enable DDR pads and set slew rate */&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;SIM_MCR |= 0xC4;&amp;nbsp;&amp;nbsp; // bits were left out of the manual so there isn't a macro right now&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_RCR |= DDR_RCR_RST_MASK;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;* (vuint32 *)(0x400Ae1ac) = 0x01030203;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR00 = 0x00000400;&amp;nbsp;&amp;nbsp;&amp;nbsp; // DDRCLS = 4 is reserved??&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR02 = 0x02000031;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR03 = 0x02020506;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR04 = 0x06090202;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR05 = 0x02020302;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR06 = 0x02904002;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR07 = 0x01000303;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR08 = 0x05030201;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR09 = 0x020000c8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR10 = 0x03003207;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR11 = 0x01000000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR12 = 0x04920031;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR13 = 0x00000005;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR14 = 0x00C80002;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR15 = 0x00000032; //&amp;nbsp; | DDR_CR15_SREF_MASK ;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR16 = 0x00000001;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR20 = 0x00030300;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR21 = 0x00040232;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR22 = 0x00000000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR23 = 0x00040302;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR25 = 0x0A010201;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR26 = 0x0101FFFF;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR27 = 0x01010101;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR28 = 0x00000003;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR29 = 0x00000000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR30 = 0x00000001;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR34 = 0x02020101;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR36 = 0x01010201;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR37 = 0x00000200;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR38 = 0x00200000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR39 = 0x01010020;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR40 = 0x00002000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR41 = 0x01010020;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR42 = 0x00002000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR43 = 0x01010020;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR44 = 0x00000000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR45 = 0x03030303;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR46 = 0x02006401;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR47 = 0x01020202;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR48 = 0x01010064;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR49 = 0x00020101;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR50 = 0x00000064;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR52 = 0x02000602;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR53 = 0x03c80000;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR54 = 0x03c803c8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR55 = 0x03c803c8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR56 = 0x020303c8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR57 = 0x01010002;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;asm("NOP");&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;DDR_CR00 |= 0x00000001;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while ((DDR_CR30 &amp;amp; 0x400) != 0x400);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;MCM_CR |= MCM_CR_DDRSIZE(1);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 06:26:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-DDR-Configuration-Issue-with-TWR-K70/m-p/721990#M44234</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-01-16T06:26:55Z</dc:date>
    </item>
  </channel>
</rss>