<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: eDMA channel idle</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-channel-idle/m-p/717113#M44003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;thanks. I'll do it If this is the only possibility...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 May 2018 15:34:51 GMT</pubDate>
    <dc:creator>martindusek</dc:creator>
    <dc:date>2018-05-24T15:34:51Z</dc:date>
    <item>
      <title>eDMA channel idle</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-channel-idle/m-p/717111#M44001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;how to check whether a dma channel is free to execute new DMA request? I thought about using ACTIVE and DONE bits of CSR register, but it seems they are not suitable for that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Checking DONE == 1 works only when there was previous DMA transaction (it doesn't work if the DMA channel hasn't been used yet).&lt;/P&gt;&lt;P&gt;And ACTIVE is set to 0 on minor loop completition. I want something that tells me all major loops (whole tranaction) has been completed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 May 2018 11:59:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-channel-idle/m-p/717111#M44001</guid>
      <dc:creator>martindusek</dc:creator>
      <dc:date>2018-05-24T11:59:12Z</dc:date>
    </item>
    <item>
      <title>Re: eDMA channel idle</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-channel-idle/m-p/717112#M44002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could do a single dummy transfer during system initialisation in order to prepare the DONE bit and then use it as flag during subsequent operations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 May 2018 15:08:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-channel-idle/m-p/717112#M44002</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-05-24T15:08:15Z</dc:date>
    </item>
    <item>
      <title>Re: eDMA channel idle</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-channel-idle/m-p/717113#M44003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;thanks. I'll do it If this is the only possibility...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 May 2018 15:34:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/eDMA-channel-idle/m-p/717113#M44003</guid>
      <dc:creator>martindusek</dc:creator>
      <dc:date>2018-05-24T15:34:51Z</dc:date>
    </item>
  </channel>
</rss>