<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C communication in Kinetis K70 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-communication-in-Kinetis-K70/m-p/716771#M43985</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;vrinda,&lt;/P&gt;&lt;P&gt;Would you please attach your project here, so that I can check it on TWR-K70F120M board.&lt;BR /&gt;Please notice:&lt;BR /&gt;The I2C bus system uses a serial data line (SDA) and a serial clock line (SCL) for data transfers.&lt;BR /&gt;All devices connected to it must have open drain or open collector outputs. A logic AND function is exercised on both lines with external pull-up resistors. The value of these resistors depends on the system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Dec 2017 07:58:58 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-12-18T07:58:58Z</dc:date>
    <item>
      <title>I2C communication in Kinetis K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-communication-in-Kinetis-K70/m-p/716770#M43984</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to establish an &lt;A class="jive-link-email-small" href="mailto:I@C"&gt;I&lt;/A&gt;2C communication between MK70FN1M0VMJ12 microcontroller of Cortex M4 architecture and slave device which is a pressure sensor. I am using Kinetis Design Studio 3.2.0 .I have used the component &lt;A class="jive-link-email-small" href="mailto:I@C_LDD"&gt;I&lt;/A&gt;2C_LDD and tried with the sample code given in help for the component&lt;/P&gt;&lt;DIV class="j-rte-table"&gt;&lt;TABLE border="0" cellpadding="0" cellspacing="0"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD align="left" style="padding-left: 15px; padding-right: 10px;" valign="top" width="100%"&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;OL&gt;&lt;LI&gt;&lt;A _jive_internal="true" class="" href="https://community.nxp.com/http://127.0.0.1:49486/help/ntopic/com.freescale.doc.processorexpert.components/Beans/I2C_LDD/I2C_LDDTypical%20Usage.html?repository=Kinetis#MasterInterrupts"&gt;Sending/Receiving data in the MASTER mode, with interrupt service&lt;/A&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;P&gt;But I am not able to get the SDA or SCL waveforms.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Dec 2017 10:32:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-communication-in-Kinetis-K70/m-p/716770#M43984</guid>
      <dc:creator>vrindamenon</dc:creator>
      <dc:date>2017-12-12T10:32:58Z</dc:date>
    </item>
    <item>
      <title>Re: I2C communication in Kinetis K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-communication-in-Kinetis-K70/m-p/716771#M43985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;vrinda,&lt;/P&gt;&lt;P&gt;Would you please attach your project here, so that I can check it on TWR-K70F120M board.&lt;BR /&gt;Please notice:&lt;BR /&gt;The I2C bus system uses a serial data line (SDA) and a serial clock line (SCL) for data transfers.&lt;BR /&gt;All devices connected to it must have open drain or open collector outputs. A logic AND function is exercised on both lines with external pull-up resistors. The value of these resistors depends on the system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Dec 2017 07:58:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-communication-in-Kinetis-K70/m-p/716771#M43985</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-12-18T07:58:58Z</dc:date>
    </item>
    <item>
      <title>Re: I2C communication in Kinetis K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-communication-in-Kinetis-K70/m-p/716772#M43986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not sure if you are test it on TWR-K70F120M board.&lt;/P&gt;&lt;P&gt;If so: [B50 B51] or [A7 A8] of J7A can be used to observe the waveform of I2C. (Please notice don't use B21 and A9 of J7A, R106 and R109 are not place by default.)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="DNP B21 A9 J7A.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30408i797D7F290B1E415A/image-size/large?v=v2&amp;amp;px=999" role="button" title="DNP B21 A9 J7A.jpg" alt="DNP B21 A9 J7A.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;There are external pull-up resistors (R54 R55) on I2C0_SCL I2C0_SDA lines at J5 on TWR-K70F120M board.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="R54 R55 J5.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30459i6F1B38ACA31FB7C5/image-size/large?v=v2&amp;amp;px=999" role="button" title="R54 R55 J5.jpg" alt="R54 R55 J5.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to your project, it seems that you are not using the &lt;A data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2F127.0.0.1%3A49486%2Fhelp%2Fntopic%2Fcom.freescale.doc.processorexpert.components%2FBeans%2FI2C_LDD%2FI2C_LDDTypical%2520Usage.html%3Frepository%3DKinetis%23MasterInterrupts" rel="nofollow" target="_blank"&gt;Sending/Receiving data in the MASTER mode, with interrupt service&lt;/A&gt; . You have Disable the interrupt service in that project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Dec 2017 02:15:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/I2C-communication-in-Kinetis-K70/m-p/716772#M43986</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-12-19T02:15:28Z</dc:date>
    </item>
  </channel>
</rss>