<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Input capture filter on FlexTimer (KV4x) in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Input-capture-filter-on-FlexTimer-KV4x/m-p/715708#M43952</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;a question regarding FTM on Kinetis:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: HelveticaLTStd-Bold; font-size: x-large;"&gt;40.4.19 Input Capture Filter Control (FTM&lt;/SPAN&gt;&lt;EM style="font-size: x-large; font-family: HelveticaLTStd-BoldObl;"&gt;x&lt;/EM&gt;&lt;SPAN style="font-family: HelveticaLTStd-Bold; font-size: x-large;"&gt;_FILTER)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;This register selects the filter value for the inputs of channels.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CHxFVAL&lt;/P&gt;&lt;P&gt;Channel&amp;nbsp;x Input Filter&lt;/P&gt;&lt;P&gt;Selects the filter value for the channel input.&lt;/P&gt;&lt;P&gt;The filter is disabled when the value is zero.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are 4 bits for the filter values. How is the "effect" of filtering per 1 LSB of those 4 bits?&lt;/P&gt;&lt;P&gt;Does it basically tell how long the input signal have to be&amp;nbsp;minimum (measured in system clock cycles) to go through the filter?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;br&lt;/P&gt;&lt;P&gt;Guenter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Oct 2017 07:14:44 GMT</pubDate>
    <dc:creator>guenter_loettrich</dc:creator>
    <dc:date>2017-10-24T07:14:44Z</dc:date>
    <item>
      <title>Input capture filter on FlexTimer (KV4x)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Input-capture-filter-on-FlexTimer-KV4x/m-p/715708#M43952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;a question regarding FTM on Kinetis:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: HelveticaLTStd-Bold; font-size: x-large;"&gt;40.4.19 Input Capture Filter Control (FTM&lt;/SPAN&gt;&lt;EM style="font-size: x-large; font-family: HelveticaLTStd-BoldObl;"&gt;x&lt;/EM&gt;&lt;SPAN style="font-family: HelveticaLTStd-Bold; font-size: x-large;"&gt;_FILTER)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;This register selects the filter value for the inputs of channels.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CHxFVAL&lt;/P&gt;&lt;P&gt;Channel&amp;nbsp;x Input Filter&lt;/P&gt;&lt;P&gt;Selects the filter value for the channel input.&lt;/P&gt;&lt;P&gt;The filter is disabled when the value is zero.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are 4 bits for the filter values. How is the "effect" of filtering per 1 LSB of those 4 bits?&lt;/P&gt;&lt;P&gt;Does it basically tell how long the input signal have to be&amp;nbsp;minimum (measured in system clock cycles) to go through the filter?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;br&lt;/P&gt;&lt;P&gt;Guenter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Oct 2017 07:14:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Input-capture-filter-on-FlexTimer-KV4x/m-p/715708#M43952</guid>
      <dc:creator>guenter_loettrich</dc:creator>
      <dc:date>2017-10-24T07:14:44Z</dc:date>
    </item>
    <item>
      <title>Re: Input capture filter on FlexTimer (KV4x)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Input-capture-filter-on-FlexTimer-KV4x/m-p/715709#M43953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Guenter,&lt;/P&gt;&lt;P&gt;For the chapter of FTM module, here the system clock means the &lt;STRONG&gt;Fast Peripheral clock&lt;/STRONG&gt;. We can find it in 'Table 6-1. Module clocks' of &lt;A href="https://www.nxp.com/docs/en/reference-manual/KV4XP100M168RM.pdf"&gt;KV4XP100M168RM&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5368iE5A785EB31D00532/image-size/large?v=v2&amp;amp;px=999" title="Table 6-1. Module clocks.png" alt="Table 6-1. Module clocks.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;For detail about the Filter, please read the '40.5.4.1 Filter for Input Capture mode'.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/5326i89682321B9F8AA1B/image-size/large?v=v2&amp;amp;px=999" title="40.5.4.1 Filter for Input Capture mode.png" alt="40.5.4.1 Filter for Input Capture mode.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Oct 2017 06:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Input-capture-filter-on-FlexTimer-KV4x/m-p/715709#M43953</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-10-26T06:42:34Z</dc:date>
    </item>
  </channel>
</rss>