<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to disable RTC module of KEA128 when i use LPO clock as the RTC clk source in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/715286#M43934</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can disable the RTC module by disable the RTC_CLKOUT pin function. Disable the &lt;SPAN class=""&gt;RTCO output function on pin PTC4 or PTC5 through SIM_PINSEL[RTCPS].&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Mar 2018 08:01:28 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2018-03-21T08:01:28Z</dc:date>
    <item>
      <title>How to disable RTC module of KEA128 when i use LPO clock as the RTC clk source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/715285#M43933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need a 3s timer and a 60s timer in different place, i choice the RTC module to generate the timer flag, LPO clk is the RTC CLK source, how to enable &amp;nbsp;RTC module when the timer is needed, and how to disable RTC when it is unwanted.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2018 02:27:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/715285#M43933</guid>
      <dc:creator>jikanghu</dc:creator>
      <dc:date>2018-03-20T02:27:09Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable RTC module of KEA128 when i use LPO clock as the RTC clk source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/715286#M43934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can disable the RTC module by disable the RTC_CLKOUT pin function. Disable the &lt;SPAN class=""&gt;RTCO output function on pin PTC4 or PTC5 through SIM_PINSEL[RTCPS].&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 08:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/715286#M43934</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2018-03-21T08:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable RTC module of KEA128 when i use LPO clock as the RTC clk source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/715287#M43935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;thanks，i don't &amp;nbsp;use RTC_CLKOUT PIN, i just use RTC as a timer, because PIT is already used , what i want to know is how to disable RTC moduel, because &amp;nbsp;i use LPOCLK as the RTC clk source, and&amp;nbsp;SIM-&amp;gt;SCGC &amp;amp;= ~SIM_SCGC_RTC_MASK will not disable RTC, is this right? the manaul says when reset ,the RTC is stopped &amp;nbsp;in default, how can i start the RTC, and when the RTC runs, how to disable it?which instruction can i use ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 09:25:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/715287#M43935</guid>
      <dc:creator>jikanghu</dc:creator>
      <dc:date>2018-03-21T09:25:12Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable RTC module of KEA128 when i use LPO clock as the RTC clk source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/715288#M43936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well, the RTC module do not need to disable, it is disabled as default. For your case, you may would like make the LPOCLK as a WDG clock. Please make reference this post on detail:&lt;A href="https://community.nxp.com/thread/448643"&gt;https://community.nxp.com/thread/448643&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2018 08:23:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/715288#M43936</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2018-06-21T08:23:38Z</dc:date>
    </item>
    <item>
      <title>Re: How to disable RTC module of KEA128 when i use LPO clock as the RTC clk source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/1277977#M60558</link>
      <description>&lt;P&gt;I want to generate RTC interrupt for every 60 seconds. Can anyone suggest how to do the register setting&lt;/P&gt;&lt;P&gt;Here is my code for 1 second interrupt&lt;/P&gt;&lt;P&gt;void init_rtc(void) {&lt;BR /&gt;SIM_SCGC |= SIM_SCGC_RTC_MASK; /* Enable clock for RTC*/&lt;BR /&gt;RTC_MOD = RTC_MOD_MOD(37500);//32000);//26666);//32000);&lt;BR /&gt;Enable_Interrupt(INT_RTC);&lt;BR /&gt;RTC_SC |= RTC_SC_RTIF_MASK | RTC_SC_RTCPS(1);&lt;BR /&gt;RTC_SC|=RTC_SC_RTCLKS(0b10); /* int clock selected*/&lt;BR /&gt;SIM_PINSEL0|=SIM_PINSEL_RTCPS_MASK; /* RTCO in PTC5 */&lt;BR /&gt;RTC_SC |=RTC_SC_RTIE_MASK;&lt;BR /&gt;}&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 06:13:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-disable-RTC-module-of-KEA128-when-i-use-LPO-clock-as-the/m-p/1277977#M60558</guid>
      <dc:creator>prasannahv</dc:creator>
      <dc:date>2021-05-18T06:13:27Z</dc:date>
    </item>
  </channel>
</rss>