<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LIN driver alters GPIO in UART mode in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-driver-alters-GPIO-in-UART-mode/m-p/712322#M43740</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply. This turned out to be an issue with my code - if the interrupt occurred at a certain point the GPIO was being left in a mess - I've restructured this part of my application and it can now ride out the interrupts without issue.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Sep 2017 07:30:58 GMT</pubDate>
    <dc:creator>ianchuter</dc:creator>
    <dc:date>2017-09-04T07:30:58Z</dc:date>
    <item>
      <title>LIN driver alters GPIO in UART mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-driver-alters-GPIO-in-UART-mode/m-p/712320#M43738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an application running which communicates successfully using the LIN driver on a&amp;nbsp;S9KEAZN16AMLH, however, while the LIN is communicating, the GPIO state is cleared apparently randomly - this stops if the LIN communication stops. The LIN is using UART, so does anyone know why it would be altering the GPIO state?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 14:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-driver-alters-GPIO-in-UART-mode/m-p/712320#M43738</guid>
      <dc:creator>ianchuter</dc:creator>
      <dc:date>2017-08-31T14:12:55Z</dc:date>
    </item>
    <item>
      <title>Re: LIN driver alters GPIO in UART mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-driver-alters-GPIO-in-UART-mode/m-p/712321#M43739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lan Chuter,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Do you mean when the LIN UART pin works, the according GPIO input status also changing?&lt;/P&gt;&lt;P&gt;&amp;nbsp; If yes, the phenomena is correct, because even you configure the pin to other modules function, the GPIO input status also works, it is correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2017 03:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-driver-alters-GPIO-in-UART-mode/m-p/712321#M43739</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-09-04T03:21:24Z</dc:date>
    </item>
    <item>
      <title>Re: LIN driver alters GPIO in UART mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-driver-alters-GPIO-in-UART-mode/m-p/712322#M43740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply. This turned out to be an issue with my code - if the interrupt occurred at a certain point the GPIO was being left in a mess - I've restructured this part of my application and it can now ride out the interrupts without issue.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2017 07:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-driver-alters-GPIO-in-UART-mode/m-p/712322#M43740</guid>
      <dc:creator>ianchuter</dc:creator>
      <dc:date>2017-09-04T07:30:58Z</dc:date>
    </item>
    <item>
      <title>Re: LIN driver alters GPIO in UART mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-driver-alters-GPIO-in-UART-mode/m-p/712323#M43741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Thanks for your updated information.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; If you still have question about it, just let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Sep 2017 08:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LIN-driver-alters-GPIO-in-UART-mode/m-p/712323#M43741</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-09-04T08:46:40Z</dc:date>
    </item>
  </channel>
</rss>