<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックGPIO at 1.4V - KEA-128</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-at-1-4V-KEA-128/m-p/711527#M43676</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am running 2 KEA128's at 3.2 V by giving VDD externally so that all the GPIO's are at 3.2v. I am using the dev boards(TRK-KEA128 boards).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From Board 1, I give input to Board 2. I make the input to board 2 from board 1 as high and low. I see that after making inputs high and low to board 2 for sometime, The voltage on board1 and board2 becomes 1.5 V while it is supposed to be zero on the corresponding pins. But if i remove the connection between the pins both pins on board 1 and board 2 are zero but if i connect it back they go to 1.5 V. Can anyone explain me the reason for this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Aug 2017 07:54:36 GMT</pubDate>
    <dc:creator>vigneshbalaji</dc:creator>
    <dc:date>2017-08-30T07:54:36Z</dc:date>
    <item>
      <title>GPIO at 1.4V - KEA-128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-at-1-4V-KEA-128/m-p/711527#M43676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am running 2 KEA128's at 3.2 V by giving VDD externally so that all the GPIO's are at 3.2v. I am using the dev boards(TRK-KEA128 boards).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From Board 1, I give input to Board 2. I make the input to board 2 from board 1 as high and low. I see that after making inputs high and low to board 2 for sometime, The voltage on board1 and board2 becomes 1.5 V while it is supposed to be zero on the corresponding pins. But if i remove the connection between the pins both pins on board 1 and board 2 are zero but if i connect it back they go to 1.5 V. Can anyone explain me the reason for this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Aug 2017 07:54:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-at-1-4V-KEA-128/m-p/711527#M43676</guid>
      <dc:creator>vigneshbalaji</dc:creator>
      <dc:date>2017-08-30T07:54:36Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO at 1.4V - KEA-128</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-at-1-4V-KEA-128/m-p/711528#M43677</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi VIGNESH BALAJI,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; This question is the same question as your another post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/459053"&gt;KEA128 GPIO at 1.4V&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please check my answer in that post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 05:32:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-at-1-4V-KEA-128/m-p/711528#M43677</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-08-31T05:32:11Z</dc:date>
    </item>
  </channel>
</rss>