<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Kinetis KL series differential ADC</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL-series-differential-ADC/m-p/710649#M43596</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is about the differential ADC built into KL series (specifically, I am interested in KL46 and KL28, but I guess the question is generic enough).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the differential ADC implemented as doing 2 single ended measurements &lt;EM&gt;very&lt;/EM&gt; quickly after each other, or is there a real differential amplifier somewhere in hardware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is a true differential measurement, then I wonder why the max and min input to the pins is specified as Vss ... 3.6V. In differential measurements, the benefit (among others) is that there can be a&amp;nbsp;DC offset on both of the differential inputs, but it will measure the difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Sep 2017 15:53:13 GMT</pubDate>
    <dc:creator>peterkisfaludi</dc:creator>
    <dc:date>2017-09-21T15:53:13Z</dc:date>
    <item>
      <title>Kinetis KL series differential ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL-series-differential-ADC/m-p/710649#M43596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is about the differential ADC built into KL series (specifically, I am interested in KL46 and KL28, but I guess the question is generic enough).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the differential ADC implemented as doing 2 single ended measurements &lt;EM&gt;very&lt;/EM&gt; quickly after each other, or is there a real differential amplifier somewhere in hardware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it is a true differential measurement, then I wonder why the max and min input to the pins is specified as Vss ... 3.6V. In differential measurements, the benefit (among others) is that there can be a&amp;nbsp;DC offset on both of the differential inputs, but it will measure the difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 15:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL-series-differential-ADC/m-p/710649#M43596</guid>
      <dc:creator>peterkisfaludi</dc:creator>
      <dc:date>2017-09-21T15:53:13Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis KL series differential ADC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL-series-differential-ADC/m-p/710650#M43597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Understood your concerning. As we know that most differential A2Ds require a true differential input to achieve the best performance. However the difference of two input of Kinetis L is limited between VREFH and VREFL. The each input voltage should limited in VDD-VSS per the data sheet. I would double check this issue and response soon.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Sep 2017 08:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL-series-differential-ADC/m-p/710650#M43597</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-09-26T08:27:19Z</dc:date>
    </item>
  </channel>
</rss>