<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KEA128 GPIO at 1.4V in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-GPIO-at-1-4V/m-p/710523#M43590</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Can you tell me the reason why i should add a 10K pull up inbetween output of board 1 and input of board 2. I want to configure software wise whether to pull up input of board 1 or pull down input of board 1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Aug 2017 11:28:50 GMT</pubDate>
    <dc:creator>vigneshbalaji</dc:creator>
    <dc:date>2017-08-30T11:28:50Z</dc:date>
    <item>
      <title>KEA128 GPIO at 1.4V</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-GPIO-at-1-4V/m-p/710521#M43588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I want to know under what conditions does KEA128 GPIO pins stay at 1.4 volts?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 12:19:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-GPIO-at-1-4V/m-p/710521#M43588</guid>
      <dc:creator>vigneshbalaji</dc:creator>
      <dc:date>2017-08-29T12:19:45Z</dc:date>
    </item>
    <item>
      <title>Re: KEA128 GPIO at 1.4V</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-GPIO-at-1-4V/m-p/710522#M43589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi VIGNESH BALAJI,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; You already ask the same two questions in the case, I post the reply in the case directly.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Please try to add an external pull up in the according pin which you are using, then check the voltage again.&lt;BR /&gt;On board output high, then other board configure the pin as GPIO input, take care, don't configure both board 1 and board 2 pin in GPIO output toghether.&lt;BR /&gt;You must configure on is GPIO output, another on is GPIO input.&lt;BR /&gt;take an example, board 1 output higher, board 2 is the GPIO input.&lt;BR /&gt;Add an external 10K pull up resistor between the board 1 and board 2, then test the voltage again, whether you still get 1.5V or you can get 3.3V.&lt;BR /&gt;Please test it at first.&lt;BR /&gt;Any updated information, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Aug 2017 08:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-GPIO-at-1-4V/m-p/710522#M43589</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-08-30T08:29:58Z</dc:date>
    </item>
    <item>
      <title>Re: KEA128 GPIO at 1.4V</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-GPIO-at-1-4V/m-p/710523#M43590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kerry,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Can you tell me the reason why i should add a 10K pull up inbetween output of board 1 and input of board 2. I want to configure software wise whether to pull up input of board 1 or pull down input of board 1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Aug 2017 11:28:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-GPIO-at-1-4V/m-p/710523#M43590</guid>
      <dc:creator>vigneshbalaji</dc:creator>
      <dc:date>2017-08-30T11:28:50Z</dc:date>
    </item>
    <item>
      <title>Re: KEA128 GPIO at 1.4V</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-GPIO-at-1-4V/m-p/710524#M43591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi VIGNESH BALAJI,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Do you try my suggestions?&lt;BR /&gt;And I don't know, whether you enable the internal pull up.&lt;BR /&gt;If you already enable the internal pull up, I think the problem is caused by the weak internal pull up resistor.&lt;BR /&gt;If you don't enable the internal pull up before, you also can try to enable the internal pull up resistor in PORT_PUEn register.&lt;BR /&gt;Please try it on your side, whether it works or not?&lt;BR /&gt;If it works, your problem is caused by the weak pull up or no pull up, the pin can't be pull to VDD because no pull up resistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 03:13:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA128-GPIO-at-1-4V/m-p/710524#M43591</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-08-31T03:13:56Z</dc:date>
    </item>
  </channel>
</rss>