<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K64 ADC specification</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-ADC-specification/m-p/709951#M43552</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please be note that Kinetis SAR only defines static performance up to 12-bit accuracy.&amp;nbsp; Ramp testing is prohibitively difficult beyond 12-bit accuracy, and although we have a capable test setup and alternative methods we could use for 16-bit linearity, the test times are so long that a full characterization of the ADC across all operating conditions and configurations is an impossible resource sink for our limited validation resources.&amp;nbsp;&amp;nbsp; That's why the K64 datasheet only provide ADC module with 12-bit mode data about TUE, DNL, INL and etc. parameters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ADC 16-bit mode should yield 12-bit accuracies performance or better. Note that although the sensitivity of the actual voltage will be 12-bit accuracy , the relative LSB will be larger because the code is in 16-bit resolution not 12-bit resolution.&lt;/P&gt;&lt;PRE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Sep 2017 08:50:09 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2017-09-25T08:50:09Z</dc:date>
    <item>
      <title>K64 ADC specification</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-ADC-specification/m-p/709950#M43551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;we use K64 in our design with the internal ADC single ended 16bit...&lt;/P&gt;&lt;P&gt;In the datasheet "K64P144M120SF5" (Rev. 7, 11/2016)&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Topic: 3.6.1.2 16-bit ADC electrical characteristics&lt;/P&gt;&lt;P&gt;There are still only values for 12-bit modes specified.&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I get valid&amp;nbsp;values for 16-bit AD-Conversion variations?&lt;/P&gt;&lt;P&gt;--&amp;gt; can&amp;nbsp;NXP provide this values? (TUE / DNL / INL / EFS)-Values for 16-bit&lt;/P&gt;&lt;P&gt;--&amp;gt; do I have to multiply the 12-bit (TUE / DNL / INL / EFS)-Values by 16&amp;nbsp; (to convert them from 12 to 16 bit??)&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've to calculate the maximum error in our circuit. External errors are known... but the internal ADC ---&amp;gt;&amp;gt; ???&lt;/P&gt;&lt;P&gt;Any hint would be appreciated!&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Manfred&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 09:42:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-ADC-specification/m-p/709950#M43551</guid>
      <dc:creator>manfredschnell</dc:creator>
      <dc:date>2017-09-21T09:42:07Z</dc:date>
    </item>
    <item>
      <title>Re: K64 ADC specification</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-ADC-specification/m-p/709951#M43552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please be note that Kinetis SAR only defines static performance up to 12-bit accuracy.&amp;nbsp; Ramp testing is prohibitively difficult beyond 12-bit accuracy, and although we have a capable test setup and alternative methods we could use for 16-bit linearity, the test times are so long that a full characterization of the ADC across all operating conditions and configurations is an impossible resource sink for our limited validation resources.&amp;nbsp;&amp;nbsp; That's why the K64 datasheet only provide ADC module with 12-bit mode data about TUE, DNL, INL and etc. parameters.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ADC 16-bit mode should yield 12-bit accuracies performance or better. Note that although the sensitivity of the actual voltage will be 12-bit accuracy , the relative LSB will be larger because the code is in 16-bit resolution not 12-bit resolution.&lt;/P&gt;&lt;PRE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2017 08:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-ADC-specification/m-p/709951#M43552</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-09-25T08:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: K64 ADC specification</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-ADC-specification/m-p/709952#M43553</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fang Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your answer.&lt;/P&gt;&lt;P&gt;Did you never run a 16-bit ADC performance test for K64?&lt;/P&gt;&lt;P&gt;If you did... would you share the results?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Otherwise I have to assume the 12-bit erros for 16-bit. (that means multiplying the brrors by 16).&lt;/P&gt;&lt;P&gt;--&amp;gt; so you should'nt write about "Two 16-bit SAR ADCs" in your datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Manfred&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2017 12:21:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-ADC-specification/m-p/709952#M43553</guid>
      <dc:creator>manfredschnell</dc:creator>
      <dc:date>2017-09-25T12:21:37Z</dc:date>
    </item>
    <item>
      <title>Re: K64 ADC specification</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-ADC-specification/m-p/709953#M43554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fang Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can you please answer?&lt;/P&gt;&lt;P&gt;It would be nice to ge a Statement about your 16-bit ADC Performance tests.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Manfred&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Nov 2017 10:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-ADC-specification/m-p/709953#M43554</guid>
      <dc:creator>manfredschnell</dc:creator>
      <dc:date>2017-11-09T10:52:50Z</dc:date>
    </item>
  </channel>
</rss>