<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: UART0 does not respond after waking up from STOP mode on Kinetis K64F</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709600#M43525</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again. I finally found my problem. The key to the problem that I was&lt;/P&gt;&lt;P&gt;having is in the following text:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;*(from the K64F RM - Chapter 25 Multipurpose Clock Generator (MCG), table&lt;/P&gt;&lt;P&gt;25-3)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;NOTE:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;*• When entering Low Power Stop modes (LLS or VLPS) from PEE mode, on exit&lt;/P&gt;&lt;P&gt;the*&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MCG clock mode is forced to PBE clock mode. C1[CLKS] and S[CLKST] will be&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;*configured to 2’b10if entering from PEE mode or to 2’b01 if entering from&lt;/P&gt;&lt;P&gt;PEI mode,*&lt;/P&gt;&lt;P&gt;*C5[PLLSTEN0] will be force to 1'b0 and S[LOCK] bit will be cleared without&lt;/P&gt;&lt;P&gt;setting*&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;S.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;*• When entering Normal Stop mode from PEE mode and if C5[PLLSTEN]=0, on&lt;/P&gt;&lt;P&gt;exit*&lt;/P&gt;&lt;P&gt;*the MCG clock mode is forced to PBE mode, the C1[CLKS] and S[CLKST] will&lt;/P&gt;&lt;P&gt;be*&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;configured to 2’b10 and S[LOCK] bit will clear without setting S[LOLS]. If&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;*C5[PLLSTEN]=1, the S[LOCK] bit will not get cleared and on exit the MCG&lt;/P&gt;&lt;P&gt;will*&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;continue to run in PEE mode.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm initialzingthe MCG clock mode to be PEE at boot time. From the note&lt;/P&gt;&lt;P&gt;above, the&lt;/P&gt;&lt;P&gt;MCG clcok mode is switched to PBE when waking up from LLS stop mode. This&lt;/P&gt;&lt;P&gt;was causing the UART and the Systick timer to stop working. All I needed to&lt;/P&gt;&lt;P&gt;do in the LLWU ISR was to set the MCG clock mode back to PEE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;German&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Tue, Aug 29, 2017 at 3:06 AM, mjbcswitzerland &amp;lt;admin@community.nxp.com&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Aug 2017 04:57:39 GMT</pubDate>
    <dc:creator>germanrivera</dc:creator>
    <dc:date>2017-08-30T04:57:39Z</dc:date>
    <item>
      <title>UART0 does not respond after waking up from STOP mode on Kinetis K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709596#M43521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Waking up after setting Sleepdeep and executing a WFI will leave UART0 unresponsive.&lt;BR /&gt;Is there anything explicit that needs to be done to make UART0 usable again?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;German&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 19:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709596#M43521</guid>
      <dc:creator>germanrivera</dc:creator>
      <dc:date>2017-08-28T19:50:29Z</dc:date>
    </item>
    <item>
      <title>Re: UART0 does not respond after waking up from STOP mode on Kinetis K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709597#M43522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi German&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following report may help:&lt;BR /&gt;&lt;A class="jive-link-thread-small" data-containerid="2019" data-containertype="14" data-objectid="327741" data-objecttype="1" href="https://community.nxp.com/thread/327741"&gt;https://community.nxp.com/message/421247&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There are binary files for the FRDM-K64F here which include low power modes for checking the UART wakeup response: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis%2FFRDM-K64F.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis/FRDM-K64F.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 23:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709597#M43522</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-08-28T23:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: UART0 does not respond after waking up from STOP mode on Kinetis K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709598#M43523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply. I had seen that post before, but it does not explain&lt;/P&gt;&lt;P&gt;if&lt;/P&gt;&lt;P&gt;something needs to be done after wake up to make the UART and Systick&lt;/P&gt;&lt;P&gt;work again. It says that in STOP mode the UART and Systick will stop&lt;/P&gt;&lt;P&gt;working, but it does not say how you make them work again after going back&lt;/P&gt;&lt;P&gt;to RUN mode. I don't need to use the UART or Systick as "wake up sources"&lt;/P&gt;&lt;P&gt;to trigger the transition from STOP mode back to RUN mode. I'm using a GPIO&lt;/P&gt;&lt;P&gt;pin interrupt as the wake up source and that is working. My problem is how&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;make the UART and Systick work again after waking up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;German&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Mon, Aug 28, 2017 at 4:05 PM, mjbcswitzerland &amp;lt;admin@community.nxp.com&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 23:56:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709598#M43523</guid>
      <dc:creator>germanrivera</dc:creator>
      <dc:date>2017-08-28T23:56:56Z</dc:date>
    </item>
    <item>
      <title>Re: UART0 does not respond after waking up from STOP mode on Kinetis K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709599#M43524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi German&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is nothing needed after returning from STOP mode to RUN mode - the clocks that had stopped will automatically be re-enabled and the peripherals fully functional again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If neither UART nor Systick are operating afterwards there must be another problem involved (eg. the GPIO wake-up may be causing the wake up to take place but not be handled correctly to allow the code to continue correctly (?)).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached is the low power control module from the uTasker project (you will see it does nothing special on return from WFI in STOP mode) as reference - you can get a complete and fully operating K64 low power solution on GITHUB or take the required pieces from it if you prefer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Aug 2017 10:05:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709599#M43524</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-08-29T10:05:51Z</dc:date>
    </item>
    <item>
      <title>Re: UART0 does not respond after waking up from STOP mode on Kinetis K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709600#M43525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again. I finally found my problem. The key to the problem that I was&lt;/P&gt;&lt;P&gt;having is in the following text:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;*(from the K64F RM - Chapter 25 Multipurpose Clock Generator (MCG), table&lt;/P&gt;&lt;P&gt;25-3)*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;NOTE:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;*• When entering Low Power Stop modes (LLS or VLPS) from PEE mode, on exit&lt;/P&gt;&lt;P&gt;the*&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;MCG clock mode is forced to PBE clock mode. C1[CLKS] and S[CLKST] will be&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;*configured to 2’b10if entering from PEE mode or to 2’b01 if entering from&lt;/P&gt;&lt;P&gt;PEI mode,*&lt;/P&gt;&lt;P&gt;*C5[PLLSTEN0] will be force to 1'b0 and S[LOCK] bit will be cleared without&lt;/P&gt;&lt;P&gt;setting*&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;S.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;*• When entering Normal Stop mode from PEE mode and if C5[PLLSTEN]=0, on&lt;/P&gt;&lt;P&gt;exit*&lt;/P&gt;&lt;P&gt;*the MCG clock mode is forced to PBE mode, the C1[CLKS] and S[CLKST] will&lt;/P&gt;&lt;P&gt;be*&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;configured to 2’b10 and S[LOCK] bit will clear without setting S[LOLS]. If&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;*C5[PLLSTEN]=1, the S[LOCK] bit will not get cleared and on exit the MCG&lt;/P&gt;&lt;P&gt;will*&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;continue to run in PEE mode.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm initialzingthe MCG clock mode to be PEE at boot time. From the note&lt;/P&gt;&lt;P&gt;above, the&lt;/P&gt;&lt;P&gt;MCG clcok mode is switched to PBE when waking up from LLS stop mode. This&lt;/P&gt;&lt;P&gt;was causing the UART and the Systick timer to stop working. All I needed to&lt;/P&gt;&lt;P&gt;do in the LLWU ISR was to set the MCG clock mode back to PEE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;German&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Tue, Aug 29, 2017 at 3:06 AM, mjbcswitzerland &amp;lt;admin@community.nxp.com&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Aug 2017 04:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709600#M43525</guid>
      <dc:creator>germanrivera</dc:creator>
      <dc:date>2017-08-30T04:57:39Z</dc:date>
    </item>
    <item>
      <title>Re: UART0 does not respond after waking up from STOP mode on Kinetis K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709601#M43526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;German&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the exit from LLS or VLPS requires the PLL to be reconfigured (if being used).&lt;/P&gt;&lt;P&gt;However, your thread suggests that you were exiting from STOP mode (sleepdeep + wfi) which is why I wrote that there is nothing else needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Aug 2017 10:14:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709601#M43526</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-08-30T10:14:34Z</dc:date>
    </item>
    <item>
      <title>Re: UART0 does not respond after waking up from STOP mode on Kinetis K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709602#M43527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;although this thread is already a year old, I'd like to add some information, because I ran into the same problem on a K22-MCU:&lt;BR /&gt;The PLL does not need to be reconfigured when trying to wake up to PEE mode (from Stop or LLS/VLPS). But the MCG_C1_CLKS does! The PLL (and OSC, etc) is restored during the power-transition, but it's output is not selected for &lt;SPAN class=""&gt;MCGOUTCLK&lt;/SPAN&gt; (25.4.1 in the reference manual of K22FN512xxx12).&lt;/P&gt;&lt;P&gt;The most simple way to achieve this is to save the C1 register before executing WFI and restoring it afterwards:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;uint8_t mcg_c1_bac &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; MCG&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;C1&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;__WFI&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
MCG&lt;SPAN class="operator token"&gt;-&amp;gt;&lt;/SPAN&gt;C1 &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; mcg_c1_bac&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;Keep in mind, that the MCG will not be configured to PEE mode until the register is restored. This means that the wake-up interrupt (and following interrupts before regular execution) will be executed in PBE mode (typically slower).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 08:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709602#M43527</guid>
      <dc:creator>schw_gld</dc:creator>
      <dc:date>2018-09-25T08:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: UART0 does not respond after waking up from STOP mode on Kinetis K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709603#M43528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the MCG configuration is a part of the recovery process and required for the final transition to PEE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; register unsigned char ucMCG_C1;
&amp;nbsp;&amp;nbsp;&amp;nbsp; ucMCG_C1 = MCG_C1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // backup the original MCG_C1 setting
...// sleep
&amp;nbsp; //LLS/VLPS sleep mode exit
&amp;nbsp;&amp;nbsp;&amp;nbsp; MCG_C5 = ((CLOCK_DIV - 1) | MCG_C5_PLLSTEN0); // move from state FEE to state PBE (or FBE) PLL remains enabled in normal stop modes
&amp;nbsp;&amp;nbsp;&amp;nbsp; MCG_C6 = ((CLOCK_MUL - MCG_C6_VDIV0_LOWEST) | MCG_C6_PLLS);
&amp;nbsp;&amp;nbsp;&amp;nbsp; while ((MCG_S &amp;amp; MCG_S_PLLST) == 0) {&amp;nbsp;&amp;nbsp;&amp;nbsp; // loop until the PLLS clock source becomes valid
&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; while ((MCG_S &amp;amp; MCG_S_LOCK) == 0) {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // loop until PLL locks
&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; MCG_C1 = ucMCG_C1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // finally move from PBE to PEE mode - switch to PLL clock (the original settings are returned)
&amp;nbsp;&amp;nbsp;&amp;nbsp; while ((MCG_S &amp;amp; MCG_S_CLKST_MASK) != MCG_S_CLKST_PLL) { // loop until the PLL clock is selected
&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PLL reconfiguration may be optional.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2018 13:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART0-does-not-respond-after-waking-up-from-STOP-mode-on-Kinetis/m-p/709603#M43528</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-09-26T13:43:16Z</dc:date>
    </item>
  </channel>
</rss>