<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K81 USB  in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-USB/m-p/706716#M43365</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thankyou Mark.&lt;/P&gt;&lt;P&gt;Plz. clarify ;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1-- If I want to use use microUSB for power and debugging. And Type A USB for Host, how can it be done. Both may be used simultaneous too.&lt;/P&gt;&lt;P&gt;2-&amp;nbsp;&amp;nbsp;Can u please help me understand your above reply with any reference design available at your end.&lt;/P&gt;&lt;P&gt;3-I am not bale to find USB pins in K81,can you plz. point it out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks to you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Sep 2017 03:59:50 GMT</pubDate>
    <dc:creator>abhishektiwari</dc:creator>
    <dc:date>2017-09-21T03:59:50Z</dc:date>
    <item>
      <title>K81 USB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-USB/m-p/706714#M43363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to design a custom board for access control using K81 secure controller. Here I wish to add two USB interfaces,One as MicroUSB (for device,can be used to power the board) and other as Type A USB(for Host). Plz. suggest how it can be done as I observes only single USB connection in controller.&lt;BR /&gt;Looking forward for early inputs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2017 08:58:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-USB/m-p/706714#M43363</guid>
      <dc:creator>abhishektiwari</dc:creator>
      <dc:date>2017-09-19T08:58:06Z</dc:date>
    </item>
    <item>
      <title>Re: K81 USB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-USB/m-p/706715#M43364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K81 has one LS/FS USB controller.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;You could use a dummy device connector just for charging and connect an OTG connector for host/device operations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternatively you may be able to connect the USB wires to two connectors as long as only one is connected at a time - in this case you may need a configuration to switch between device and host modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 11:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-USB/m-p/706715#M43364</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-09-20T11:04:54Z</dc:date>
    </item>
    <item>
      <title>Re: K81 USB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-USB/m-p/706716#M43365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thankyou Mark.&lt;/P&gt;&lt;P&gt;Plz. clarify ;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1-- If I want to use use microUSB for power and debugging. And Type A USB for Host, how can it be done. Both may be used simultaneous too.&lt;/P&gt;&lt;P&gt;2-&amp;nbsp;&amp;nbsp;Can u please help me understand your above reply with any reference design available at your end.&lt;/P&gt;&lt;P&gt;3-I am not bale to find USB pins in K81,can you plz. point it out.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks to you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 03:59:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-USB/m-p/706716#M43365</guid>
      <dc:creator>abhishektiwari</dc:creator>
      <dc:date>2017-09-21T03:59:50Z</dc:date>
    </item>
    <item>
      <title>Re: K81 USB</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-USB/m-p/706717#M43366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe you could put an OpenSDA K20 on the board to give it debugging capability and USB device - then use the K81's USB as host on the other connector?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB pins are called USB0_DP and USB0_DM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis%2FFRDM-K82F.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis/FRDM-K82F.html&lt;/A&gt;&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis%2FTWR-K80F150M.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis/TWR-K80F150M.html&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 23:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K81-USB/m-p/706717#M43366</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-09-21T23:20:19Z</dc:date>
    </item>
  </channel>
</rss>