<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Minimum VDD for USB device</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Minimum-VDD-for-USB-device/m-p/706527#M43352</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is minimum voltage for MKL27Z64VLH4 (or similar M0+) to work as USB device? Is it possible to use it as 1.8V like on attached picture?&lt;/P&gt;&lt;P&gt;If I understood right, during working as crystalless USB device, internal precise 48 MHz clock can be used also as source for master (or for other peripherals) clock.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found FlexIO AN for UART, I2C, SPI, PWM. Is there any FlexIO SWD (master) open source example?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Sep 2017 11:33:20 GMT</pubDate>
    <dc:creator>jh0</dc:creator>
    <dc:date>2017-09-18T11:33:20Z</dc:date>
    <item>
      <title>Minimum VDD for USB device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Minimum-VDD-for-USB-device/m-p/706527#M43352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is minimum voltage for MKL27Z64VLH4 (or similar M0+) to work as USB device? Is it possible to use it as 1.8V like on attached picture?&lt;/P&gt;&lt;P&gt;If I understood right, during working as crystalless USB device, internal precise 48 MHz clock can be used also as source for master (or for other peripherals) clock.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I found FlexIO AN for UART, I2C, SPI, PWM. Is there any FlexIO SWD (master) open source example?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 11:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Minimum-VDD-for-USB-device/m-p/706527#M43352</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2017-09-18T11:33:20Z</dc:date>
    </item>
    <item>
      <title>Re: Minimum VDD for USB device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Minimum-VDD-for-USB-device/m-p/706528#M43353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px; font-family: arial,helvetica,sans-serif;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN style="font-size: 15px; font-family: arial,helvetica,sans-serif;"&gt;yes, the internal USB regulator powers the USB transceiver or the MCU itself (depending on the application). 
in this case the supply voltage for chip could be 1.8V.&amp;nbsp; &lt;/SPAN&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 08:53:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Minimum-VDD-for-USB-device/m-p/706528#M43353</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-09-21T08:53:41Z</dc:date>
    </item>
    <item>
      <title>Re: Minimum VDD for USB device</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Minimum-VDD-for-USB-device/m-p/706529#M43354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If communicating via USB the minimum voltage per the standard is 4.2V for VBus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.usb.org/developers/docs/whitepapers/power_delivery_motherboards.pdf"&gt;http://www.usb.org/developers/docs/whitepapers/power_delivery_motherboards.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I know you said Device, understating the Host end is important as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.usb.org/developers/compliance/electrical_tests/USB_2_0_Electrical_Compliance_Specification.pdf"&gt;http://www.usb.org/developers/compliance/electrical_tests/USB_2_0_Electrical_Compliance_Specification.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See &lt;A href="http://www.usb.org"&gt;http://www.usb.org&lt;/A&gt; for others.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Sep 2017 17:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Minimum-VDD-for-USB-device/m-p/706529#M43354</guid>
      <dc:creator>bobpaddock</dc:creator>
      <dc:date>2017-09-21T17:20:26Z</dc:date>
    </item>
  </channel>
</rss>