<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB MBED DISCONNECTS WHEN PUTTING A .BIN FILE IN THE MBED FOLDER in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MBED-DISCONNECTS-WHEN-PUTTING-A-BIN-FILE-IN-THE-MBED-FOLDER/m-p/704537#M43255</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I tried to put a .bin file to the USB MBED folders of&amp;nbsp; FRDM k22&amp;nbsp; in a linux environment , the folder disconnected immediately , and then after a while , it reconnected and showed the icon on the file system, but the .bin file vanished.&lt;/P&gt;&lt;P&gt;Is the ARM MBED stable in K22F?&amp;nbsp; do you have a solution for this kind of problem.&amp;nbsp;&amp;nbsp; Also i tried to draw the newest bootloader firmware to the bootloader folder, it did the same.&lt;/P&gt;&lt;P&gt;Also can you tell me when the .bin will be loaded to the ARM flash ,when the reset button is pressed ? or ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Oct 2017 23:00:45 GMT</pubDate>
    <dc:creator>alvenwu</dc:creator>
    <dc:date>2017-10-11T23:00:45Z</dc:date>
    <item>
      <title>USB MBED DISCONNECTS WHEN PUTTING A .BIN FILE IN THE MBED FOLDER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MBED-DISCONNECTS-WHEN-PUTTING-A-BIN-FILE-IN-THE-MBED-FOLDER/m-p/704537#M43255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I tried to put a .bin file to the USB MBED folders of&amp;nbsp; FRDM k22&amp;nbsp; in a linux environment , the folder disconnected immediately , and then after a while , it reconnected and showed the icon on the file system, but the .bin file vanished.&lt;/P&gt;&lt;P&gt;Is the ARM MBED stable in K22F?&amp;nbsp; do you have a solution for this kind of problem.&amp;nbsp;&amp;nbsp; Also i tried to draw the newest bootloader firmware to the bootloader folder, it did the same.&lt;/P&gt;&lt;P&gt;Also can you tell me when the .bin will be loaded to the ARM flash ,when the reset button is pressed ? or ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 23:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MBED-DISCONNECTS-WHEN-PUTTING-A-BIN-FILE-IN-THE-MBED-FOLDER/m-p/704537#M43255</guid>
      <dc:creator>alvenwu</dc:creator>
      <dc:date>2017-10-11T23:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: USB MBED DISCONNECTS WHEN PUTTING A .BIN FILE IN THE MBED FOLDER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MBED-DISCONNECTS-WHEN-PUTTING-A-BIN-FILE-IN-THE-MBED-FOLDER/m-p/704538#M43256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Experienced environment : Linux 4.12.11&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; openSDA 2.1&amp;nbsp;&amp;nbsp;&amp;nbsp; CMSIS-DAP 100&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 04:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MBED-DISCONNECTS-WHEN-PUTTING-A-BIN-FILE-IN-THE-MBED-FOLDER/m-p/704538#M43256</guid>
      <dc:creator>alvenwu</dc:creator>
      <dc:date>2017-10-12T04:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: USB MBED DISCONNECTS WHEN PUTTING A .BIN FILE IN THE MBED FOLDER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MBED-DISCONNECTS-WHEN-PUTTING-A-BIN-FILE-IN-THE-MBED-FOLDER/m-p/704539#M43257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alven,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure if you have checked the &lt;A href="https://www.nxp.com/products/microcontrollers-and-processors/arm-based-processors-and-mcus/kinetis-cortex-m-mcus/developer-resources/ides-for-kinetis-mcus/opensda-serial-and-debug-adapter:OPENSDA?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1#FRDM-K22F"&gt;OpenSDA link&lt;/A&gt; at NXP website before.&lt;/P&gt;&lt;P&gt;There provided the DAPLink OpenSDA V2.2 bootloader image and latest firmware.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Oct 2017 06:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-MBED-DISCONNECTS-WHEN-PUTTING-A-BIN-FILE-IN-THE-MBED-FOLDER/m-p/704539#M43257</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-10-16T06:23:42Z</dc:date>
    </item>
  </channel>
</rss>