<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB examples on FRDM-K28F not working in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-examples-on-FRDM-K28F-not-working/m-p/704397#M43251</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, please try with attached image file.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Oct 2017 07:05:04 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2017-10-20T07:05:04Z</dc:date>
    <item>
      <title>USB examples on FRDM-K28F not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-examples-on-FRDM-K28F-not-working/m-p/704394#M43248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;we are evaluating the FRDM-K28F for a HS USB application. But no matter what I try, I can't get USB working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The blink example works nicely ;-) &amp;nbsp; When I try any of the other USB examples USB never is recognized. Linux lsusb does not change when I attach the USB cable to the "HS USB" port, the USB attach sound is never played. I especially tried the usb_device_cdc_vcom example. The software on the board seems to run nicely, AppTask is repeated in the main loop.&lt;BR /&gt;I understand, that there is at least one jumper, which has to be set right ( J53 open?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using SDK_2.2_FRDM-K28F, downloaded recently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I compared usb_device_config with the K64F project and even tried to use this file since it seems to have helped others, but no change.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also I have the impression that USBPHYPLLCLK should be active in the configuration ( MCUXpresso config tools doesn't show it as active, but I didn't check if it was activated by some init in SW, which would make sense. Activating this clock in MCUXpresso doesn't change anything).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody have any clue what is going wrong or what else I can check?&lt;BR /&gt;Knowing proven good jumper setting would help too.&lt;BR /&gt;Or maybe there is a .bin so I can check if there is something wrong with my hw?&lt;/P&gt;&lt;P&gt;I feel quite a bit stuck at the moment and would appreciate any help a lot !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your clues 8^)&lt;BR /&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 08:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-examples-on-FRDM-K28F-not-working/m-p/704394#M43248</guid>
      <dc:creator>marzl</dc:creator>
      <dc:date>2017-10-12T08:20:13Z</dc:date>
    </item>
    <item>
      <title>Re: USB examples on FRDM-K28F not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-examples-on-FRDM-K28F-not-working/m-p/704395#M43249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried the [usb_device_cdc_vcom] demo, the FRDM-K28F J14 jumper On and J53 jumper Off.&lt;/P&gt;&lt;P&gt;Please check below picture:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30150i8763B312B7EE2C9B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After that, you could find the virtual serial port at [Computer Management] panel:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30198i5BDB8D01C78A5EDE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Oct 2017 07:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-examples-on-FRDM-K28F-not-working/m-p/704395#M43249</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-10-13T07:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: USB examples on FRDM-K28F not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-examples-on-FRDM-K28F-not-working/m-p/704396#M43250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ma Hui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks so much for your fast response!&lt;BR /&gt;But unfortunately my FRDM-K28F is still not recognized by the PC as a USB device, even if I started a new copy of the example project and set the jumpers and cable as you did :-(&amp;nbsp; I hope, I didn't wreck the board somehow previously. Would you mind to send me your binary .bin of the project, please? If I understood that right I would only have to copy it to the USB-folder which appears when connecting to the debug port of the device. It would help me a lot to track the problem ;-)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again for your help!&lt;BR /&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 11:10:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-examples-on-FRDM-K28F-not-working/m-p/704396#M43250</guid>
      <dc:creator>marzl</dc:creator>
      <dc:date>2017-10-19T11:10:26Z</dc:date>
    </item>
    <item>
      <title>Re: USB examples on FRDM-K28F not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-examples-on-FRDM-K28F-not-working/m-p/704397#M43251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, please try with attached image file.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Oct 2017 07:05:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-examples-on-FRDM-K28F-not-working/m-p/704397#M43251</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-10-20T07:05:04Z</dc:date>
    </item>
  </channel>
</rss>