<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KL27Z256VFT4 Using external reference on VREFH? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z256VFT4-Using-external-reference-on-VREFH/m-p/704226#M43231</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Seth,&lt;/P&gt;&lt;P&gt;This device contains dedicated VREFH and VREFL pins on 64-pin and 48-pin(KL27Z256VFT4) packages.&lt;/P&gt;&lt;P&gt;So I think it's ok to use external reference on VREFH.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29436i6C8352FD63942F2E/image-size/large?v=v2&amp;amp;px=999" title="23.1.4 ADC analog supply and reference connections.png" alt="23.1.4 ADC analog supply and reference connections.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The output of On-chip 1.2V high precision voltage reference VREF_OUT shares with VREFH on 64-pin and 48-pin&amp;nbsp; packages. When VREF_OUT is enabled, this pin needs to connect a capacitor to ground.&lt;/P&gt;&lt;P&gt;So you need to check if it was disabled or not.(SIM_SCGC4[VREF]=0)&lt;/P&gt;&lt;P&gt;And set ADCx_SC2[REFSEL]=00 Default voltage reference pin pair, that is, external pins VREFH and VREFL&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29453iA02DDD72A41448E4/image-size/large?v=v2&amp;amp;px=999" title="2.3.2 Analog reference options.png" alt="2.3.2 Analog reference options.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are testing the adc example in &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-333304"&gt;SDK2.x&lt;/A&gt;, please notice the '#define BOARD_ADC_USE_ALT_VREF 1U' in board.h&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29561i66BAFB7211BFA2A6/image-size/large?v=v2&amp;amp;px=999" title="BOARD_ADC_USE_ALT_VREF.png" alt="BOARD_ADC_USE_ALT_VREF.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please connect 1v at ADC input pin, what value will you get?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Sep 2017 09:33:29 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-09-15T09:33:29Z</dc:date>
    <item>
      <title>KL27Z256VFT4 Using external reference on VREFH?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z256VFT4-Using-external-reference-on-VREFH/m-p/704225#M43230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the KL27Z256VFT4 in a project currently in development.&amp;nbsp; It seems that the VREFH cannot be used with an external reference.&amp;nbsp; When attempting to use a 2.5 volt reference connected to VREFH the adc conversion consistently reads 0xFF.&amp;nbsp; I have verified that the internal reference is off and that the source for the ADC reference is set to the VREFH/VREFL pair.&amp;nbsp; Is there something I am missing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Sep 2017 16:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z256VFT4-Using-external-reference-on-VREFH/m-p/704225#M43230</guid>
      <dc:creator>codemonk</dc:creator>
      <dc:date>2017-09-14T16:05:40Z</dc:date>
    </item>
    <item>
      <title>Re: KL27Z256VFT4 Using external reference on VREFH?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z256VFT4-Using-external-reference-on-VREFH/m-p/704226#M43231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Seth,&lt;/P&gt;&lt;P&gt;This device contains dedicated VREFH and VREFL pins on 64-pin and 48-pin(KL27Z256VFT4) packages.&lt;/P&gt;&lt;P&gt;So I think it's ok to use external reference on VREFH.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29436i6C8352FD63942F2E/image-size/large?v=v2&amp;amp;px=999" title="23.1.4 ADC analog supply and reference connections.png" alt="23.1.4 ADC analog supply and reference connections.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The output of On-chip 1.2V high precision voltage reference VREF_OUT shares with VREFH on 64-pin and 48-pin&amp;nbsp; packages. When VREF_OUT is enabled, this pin needs to connect a capacitor to ground.&lt;/P&gt;&lt;P&gt;So you need to check if it was disabled or not.(SIM_SCGC4[VREF]=0)&lt;/P&gt;&lt;P&gt;And set ADCx_SC2[REFSEL]=00 Default voltage reference pin pair, that is, external pins VREFH and VREFL&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29453iA02DDD72A41448E4/image-size/large?v=v2&amp;amp;px=999" title="2.3.2 Analog reference options.png" alt="2.3.2 Analog reference options.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are testing the adc example in &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-333304"&gt;SDK2.x&lt;/A&gt;, please notice the '#define BOARD_ADC_USE_ALT_VREF 1U' in board.h&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29561i66BAFB7211BFA2A6/image-size/large?v=v2&amp;amp;px=999" title="BOARD_ADC_USE_ALT_VREF.png" alt="BOARD_ADC_USE_ALT_VREF.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please connect 1v at ADC input pin, what value will you get?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Sep 2017 09:33:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL27Z256VFT4-Using-external-reference-on-VREFH/m-p/704226#M43231</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-09-15T09:33:29Z</dc:date>
    </item>
  </channel>
</rss>