<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 MK20DX256VMC7 IDD_VBAT when VDD = 0</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX256VMC7-IDD-VBAT-when-VDD-0/m-p/703683#M43218</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you confirm that the RTC of MK20DX256&amp;nbsp; can still run on Vbat voltage even if main MCU Vdd = 0 , and then IDD_VBAT average current is Max 0.94µA at 3.0V, –40 to 25°C, according to datasheet?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Philippe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Aug 2017 17:44:22 GMT</pubDate>
    <dc:creator>phil74</dc:creator>
    <dc:date>2017-08-21T17:44:22Z</dc:date>
    <item>
      <title>MK20DX256VMC7 IDD_VBAT when VDD = 0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX256VMC7-IDD-VBAT-when-VDD-0/m-p/703683#M43218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you confirm that the RTC of MK20DX256&amp;nbsp; can still run on Vbat voltage even if main MCU Vdd = 0 , and then IDD_VBAT average current is Max 0.94µA at 3.0V, –40 to 25°C, according to datasheet?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Philippe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Aug 2017 17:44:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX256VMC7-IDD-VBAT-when-VDD-0/m-p/703683#M43218</guid>
      <dc:creator>phil74</dc:creator>
      <dc:date>2017-08-21T17:44:22Z</dc:date>
    </item>
    <item>
      <title>Re: MK20DX256VMC7 IDD_VBAT when VDD = 0</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX256VMC7-IDD-VBAT-when-VDD-0/m-p/703684#M43219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, that operational understanding is correct.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Aug 2017 10:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK20DX256VMC7-IDD-VBAT-when-VDD-0/m-p/703684#M43219</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2017-08-22T10:35:38Z</dc:date>
    </item>
  </channel>
</rss>