<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K66 Flexbus, multiplexed and non multiplexed mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Flexbus-multiplexed-and-non-multiplexed-mode/m-p/703652#M43216</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Flexbus non-multiplexed mode or multiplexed mode based on chip pin resource.&lt;/P&gt;&lt;P&gt;The 32-bit data port non-multiplexed mode need use splitted address line, while&amp;nbsp; MK66FX1M0VMD18&amp;nbsp; doesn't provide enough splitted Flexbus address pins, which missing FB_A[15:0].&lt;/P&gt;&lt;P&gt;So, MK66FX1M0VMD18&amp;nbsp; doesn't support 32-bit data port non-multiplexed mode.&lt;/P&gt;&lt;P&gt;Customer can only use Flexbus with 32-bit data port multiplexed mode.&lt;/P&gt;&lt;P&gt;There is an application note AN4393 about Flexbus function, please check &lt;A href="http://cache.nxp.com/docs/en/application-note/AN4393.pdf"&gt;here&lt;/A&gt; for detailed info.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Aug 2017 05:30:19 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2017-08-23T05:30:19Z</dc:date>
    <item>
      <title>K66 Flexbus, multiplexed and non multiplexed mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Flexbus-multiplexed-and-non-multiplexed-mode/m-p/703651#M43215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to flexbus usage and I don't understand how the K66 chooses between multiplexed and non multiplexed mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using a MK66FX1M0VMD18 and according to reference manual, it support both multiplexed and non multiplexed 32-bit address and 32-bit data busses. The little note "Some modes of operation (like 32-bit non-multiplexed address and data busses) require signals to actually be available on the pins of your specific device package" does not really help because I have not seen anywhere a list of the required pins for the non-multiplexed mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to configure FB_CSCR0 with BLS=1, AA=1 and PS=0 (I also tried 1 and 2) but I seem to remains in multiplexed mode. FB_CSAR0=0x6000_0000, FB_CSMR0=0x0000_0001 =&amp;gt; 64KB block @0x6000_0000. CSPMCR = 0x0222_2000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried FB_CSCR0 with BLS=1, AA=1, PS=1 (8 bits) with CSPMCR = 0x0200_0000 without any success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone give a working example or explanation of the minimal settings required to use non-multiplexed 32-bit address and 32-bit data busses ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Aug 2017 08:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Flexbus-multiplexed-and-non-multiplexed-mode/m-p/703651#M43215</guid>
      <dc:creator>tatalifaku</dc:creator>
      <dc:date>2017-08-22T08:14:22Z</dc:date>
    </item>
    <item>
      <title>Re: K66 Flexbus, multiplexed and non multiplexed mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Flexbus-multiplexed-and-non-multiplexed-mode/m-p/703652#M43216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Flexbus non-multiplexed mode or multiplexed mode based on chip pin resource.&lt;/P&gt;&lt;P&gt;The 32-bit data port non-multiplexed mode need use splitted address line, while&amp;nbsp; MK66FX1M0VMD18&amp;nbsp; doesn't provide enough splitted Flexbus address pins, which missing FB_A[15:0].&lt;/P&gt;&lt;P&gt;So, MK66FX1M0VMD18&amp;nbsp; doesn't support 32-bit data port non-multiplexed mode.&lt;/P&gt;&lt;P&gt;Customer can only use Flexbus with 32-bit data port multiplexed mode.&lt;/P&gt;&lt;P&gt;There is an application note AN4393 about Flexbus function, please check &lt;A href="http://cache.nxp.com/docs/en/application-note/AN4393.pdf"&gt;here&lt;/A&gt; for detailed info.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 05:30:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Flexbus-multiplexed-and-non-multiplexed-mode/m-p/703652#M43216</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-08-23T05:30:19Z</dc:date>
    </item>
    <item>
      <title>Re: K66 Flexbus, multiplexed and non multiplexed mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Flexbus-multiplexed-and-non-multiplexed-mode/m-p/703653#M43217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, now, I understand why I'm stuck in multiplexed mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact, AN4393 is a bit a reason of my misunderstanding. It tried to create something like the LCD example but in non multiplexed mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 07:31:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Flexbus-multiplexed-and-non-multiplexed-mode/m-p/703653#M43217</guid>
      <dc:creator>tatalifaku</dc:creator>
      <dc:date>2017-08-23T07:31:52Z</dc:date>
    </item>
  </channel>
</rss>