<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Freedom KL27 external GPIO Interrupt</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703495#M43210</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked your binary and can tell you the problem:&lt;/P&gt;&lt;P&gt;1. The Port and its interrupt (also in NVIC) is set up correctly.&lt;BR /&gt;2. The interrupt fires and its vector is taken, however you haven't installed the correct handler since it calls the "un-handled" interrupt which means that it hangs in the interrupt forever (with KDS you should have been able to see this too).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is easy to see that the vectors are missing (you have VTOR set to 0 - meaning that the vectors are hard-coded - you will probably find them in an assembler file somewhere).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the values that you have in Flash starting at address 0x00000000. I have labeled the vectors of interest, including the location of the "port B,C,D,E" interrupt vector (the last one).&lt;BR /&gt;Since the vector value is the same as many others it is clear that a un-handled (default) vector is being used rather than one to handle the port interrupt.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30062i7B49297ACF246C1A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;These are the values that you have in Flash starting at address 0x00000000. I have labeled the vectors of interest, including the location of the "port B,C,D,E" interrupt vector (the last one).&lt;BR /&gt;Since the vector value is the same as many others it is clear that a un-handled (default) vector is being used rather than one to handle the port interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you can work out why and where you need to add it you should be OK. You will however need to ensure that the handler used is suitable for a port interrupt shared by these 4 ports or, in the worst case, one that at least handles the port C case for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As noted before, if you would prefer a more power ful and fool-proof solution just down-load the (free) Open Source uTasker project since it handles all such details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Oct 2017 20:10:49 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2017-10-12T20:10:49Z</dc:date>
    <item>
      <title>Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703486#M43201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a FRDM-K27Z board and want to use a external GPIO Interrupt on PTC3. For testing the GPIO Interrupt i use the Switch 3 on the PTC1. I have the problem, that the Interrupt is never called. I used the example of the KSDK 2.0 and made minimal changes but the Interrupt Function is never called.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below you can see the code i used. Maybe you can find some errors in that code or help me otherwise.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_debug_console.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_port.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_gpio.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_common.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"board.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"pin_mux.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"fsl_device_registers.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;&amp;lt;stdbool.h&amp;gt;&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"clock_config.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/*******************************************************************************
 * Definitions
 ******************************************************************************/&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define BOARD_LED_GPIO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_LED_RED_GPIO&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define BOARD_LED_GPIO_PIN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_LED_RED_GPIO_PIN&lt;/SPAN&gt;

&lt;SPAN class="property macro token"&gt;#define BOARD_SW_GPIO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_SW3_GPIO&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define BOARD_SW_PORT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_SW3_PORT&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define BOARD_SW_GPIO_PIN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_SW3_GPIO_PIN&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define BOARD_SW_IRQ&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_SW3_IRQ&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define BOARD_SW_IRQ_HANDLER&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_SW3_IRQ_HANDLER&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define BOARD_SW_NAME&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BOARD_SW3_NAME&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/*******************************************************************************
 * Prototypes
 ******************************************************************************/&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/*******************************************************************************
 * Variables
 ******************************************************************************/&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Whether the SW button is pressed */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;volatile&lt;/SPAN&gt; bool g_ButtonPress &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; false&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/*******************************************************************************
 * Code
 ******************************************************************************/&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/*!
 * @brief Interrupt service fuction of switch.
 *
 * This function toggles the LED
 */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;BOARD_SW_IRQ_HANDLER&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Clear external interrupt flag. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;GPIO_ClearPinsInterruptFlags&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;BOARD_SW_GPIO&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1U&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; BOARD_SW_GPIO_PIN&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Change state of button. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; g_ButtonPress &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; true&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;PRINTF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"\r\n Interrupt Occurred\r\n"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Toggle LED. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;GPIO_TogglePinsOutput&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;BOARD_LED_GPIO&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1U&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; BOARD_LED_GPIO_PIN&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/*!
 * @brief Main function
 */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;main&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Define the init structure for the input switch pin */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; gpio_pin_config_t sw_config &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kGPIO_DigitalInput&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Define the init structure for the output LED pin */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; gpio_pin_config_t led_config &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; kGPIO_DigitalOutput&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;BOARD_InitPins&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;BOARD_BootClockRUN&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//Changed from BOARD_BootClockHSRUN(); &lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;BOARD_InitDebugConsole&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;CLOCK_EnableClock&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;kCLOCK_PortA&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;CLOCK_EnableClock&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;kCLOCK_PortB&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;CLOCK_EnableClock&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;kCLOCK_PortC&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Print a note to terminal. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;PRINTF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"\r\n GPIO Driver example\r\n"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;PRINTF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;"\r\n Press %s to turn on/off a LED \r\n"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; BOARD_SW_NAME&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Init input switch GPIO. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;PORT_SetPinInterruptConfig&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;BOARD_SW_PORT&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; BOARD_SW_GPIO_PIN&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; kPORT_InterruptFallingEdge&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;EnableIRQ&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;BOARD_SW_IRQ&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;GPIO_PinInit&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;BOARD_SW_GPIO&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; BOARD_SW_GPIO_PIN&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;sw_config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Init output LED GPIO. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;GPIO_PinInit&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;BOARD_LED_GPIO&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; BOARD_LED_GPIO_PIN&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;led_config&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;g_ButtonPress&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="token function"&gt;PRINTF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="string token"&gt;" %s is pressed \r\n"&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; BOARD_SW_NAME&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="comment token"&gt;/* Reset state of button. */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; g_ButtonPress &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; false&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="line-numbers-rows"&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Killerawft&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Edit: I also tested the SW3 itself and the switch worked fine without an Interrupt so the error must be in my code.&lt;/P&gt;&lt;P&gt;Edit 2: i tested the same Code as above with the SW1 and the line&amp;nbsp;&lt;/P&gt;&lt;P&gt;PORT_SetPinMux(BOARD_SW_PORT, BOARD_SW_GPIO_PIN, kPORT_MuxAsGpio);&lt;/P&gt;&lt;P&gt;after line 80 and that worked. So I can call the Interrupt of the Port A with my Code, but i need to Call an Interrupt with the Port C GPIO.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337713" rel="nofollow noopener noreferrer" target="_blank"&gt;gpio_interrupt.elf.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Oct 2017 13:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703486#M43201</guid>
      <dc:creator>killerawft</dc:creator>
      <dc:date>2017-10-11T13:16:31Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703487#M43202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;See this video concerning details about the port interrupts on the KL27: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fyoutu.be%2FCubinvMuTwU" rel="nofollow" target="_blank"&gt;https://youtu.be/CubinvMuTwU&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached is a binary that you can load to your board which prints out a message each time it is pressed (using falling edge interrupt detection) [openSDA VCOM at 115200Baud].&lt;BR /&gt;In addition, it includes USB-CDC on USB0 which also prints out the same message when connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Notes:&lt;BR /&gt;- The KL27 has a single shared interrupt for ports B,C,D and E, which may be the source of your difficulty&lt;BR /&gt;- There is a memory debugger on the command line interface (binary attached) which can be used for viewing registers so you can compare content with your setup to find a deviation.&lt;BR /&gt;&lt;SPAN&gt;- At &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;SPAN&gt; you can use the uTasker open source project as reference to solving such issues - in Visual Studio you can simulate the GPIO interrupt operations and solve any complications with the libraries that you may otherwise be using.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KL27 References:&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis%2FFRDM-KL27Z.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis/FRDM-KL27Z.html&lt;/A&gt;&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis%2FCapuccino-KL27.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis/Capuccino-KL27.html&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 00:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703487#M43202</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-10-12T00:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703488#M43203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I watched the video and added the line PORT_SetPinMux(BOARD_SW_PORT, BOARD_SW_GPIO_PIN, kPORT_MuxAsGpio); &lt;SPAN&gt;a&lt;/SPAN&gt;&lt;SPAN&gt;f&lt;/SPAN&gt;&lt;SPAN&gt;ter line 80&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;to set the Port as a&amp;nbsp;&lt;SPAN&gt;GPIO and now the ISFR re&lt;SPAN&gt;gister&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;of Port C is set. That wasnt the case before. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I also saw that the highest bit of the NVIC_ISER and the NVIC_ICER registers are set. Shouldnt the&amp;nbsp;NVIC_ICER re&lt;SPAN&gt;gister cleared since that &lt;SPAN&gt;re&lt;/SPAN&gt;&lt;SPAN&gt;gister&lt;SPAN&gt;&amp;nbsp;disables the interrupt? Clearing it by hand with&amp;nbsp;NVIC-&amp;gt;ICER[0U] = 0; didnt worked.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;And i couldnt test your binary file because i dont know how to flash it to the ARM with the&amp;nbsp;Kinetis Design Studio 3 IDE, so i couldnt test that.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 01:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703488#M43203</guid>
      <dc:creator>killerawft</dc:creator>
      <dc:date>2017-10-12T01:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703489#M43204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NVIC_ISER and NVIC_ICER always just READ the contents of what is enabled -- they are not themselves registers, they are access-means to 'set' or 'clear' bits in the ONE physical 'enable' register --- you 'write 1 bits' into these addresses to (individually) enable or disable (Set or Clear each 'enable' bit).&amp;nbsp; Your write of 'zero' had no effect; you would need to write 1&amp;lt;&amp;lt;31 into ICER to disable a PortC/D interrupt.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 17:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703489#M43204</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2017-10-12T17:12:20Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703490#M43205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try to do GPIO_PinInit before PORT_SetPinInterruptConfig to see if that helps:&lt;/P&gt;&lt;PRE class="" style="color: #000000; background: #f5f2f0; border: 0px; margin: 0.5em 0px; padding: 1em 1em 1em 3.8em;"&gt;&lt;CODE style="border: 0px; font-weight: inherit;"&gt;&lt;SPAN class="" style="color: #d74444; border: 0px; font-weight: inherit;"&gt;&lt;SPAN class="" style="border: 0px; font-weight: inherit;"&gt;GPIO_PinInit&lt;/SPAN&gt;&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;(&lt;/SPAN&gt;BOARD_SW_GPIO&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;,&lt;/SPAN&gt; BOARD_SW_GPIO_PIN&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;,&lt;/SPAN&gt; &lt;SPAN class="" style="color: #a67f59; background: rgba(255, 255, 255, 0.5); border: 0px; font-weight: inherit;"&gt;&amp;amp;&lt;/SPAN&gt;sw_config&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;)&lt;/SPAN&gt;&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;;&lt;/SPAN&gt;
PORT_SetPinInterruptConfig&lt;/SPAN&gt;&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;(&lt;/SPAN&gt;BOARD_SW_PORT&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;,&lt;/SPAN&gt; BOARD_SW_GPIO_PIN&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;,&lt;/SPAN&gt; kPORT_InterruptFallingEdge&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;)&lt;/SPAN&gt;&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="" style="color: #d74444; border: 0px; font-weight: inherit;"&gt;EnableIRQ&lt;/SPAN&gt;&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;(&lt;/SPAN&gt;BOARD_SW_IRQ&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;)&lt;/SPAN&gt;&lt;SPAN class="" style="color: #999999; border: 0px; font-weight: inherit;"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 17:34:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703490#M43205</guid>
      <dc:creator>danieltruong</dc:creator>
      <dc:date>2017-10-12T17:34:42Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703491#M43206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the mean time i also found that out but thanks for that advice.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 17:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703491#M43206</guid>
      <dc:creator>killerawft</dc:creator>
      <dc:date>2017-10-12T17:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703492#M43207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately that didnt helped either.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 17:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703492#M43207</guid>
      <dc:creator>killerawft</dc:creator>
      <dc:date>2017-10-12T17:39:16Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703493#M43208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You don't need KDS to flash binaries to a FRDM board: Just drag and drop it to the hard drive that appears when the board is plugged in.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can also build the projects yourself with the KDS project on GITHUB. Or do the same in its simulator, in order to improve development efficiency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;PS. If you do don't manage to sort it out attach your binary and I'll tell you what is wrong.&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 17:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703493#M43208</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-10-12T17:53:30Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703494#M43209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I&amp;nbsp;loaded your binary to the controller and when i pressed SW3 the Interrupt printed a message. In the Question i added the binary of my code so you can check it.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 18:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703494#M43209</guid>
      <dc:creator>killerawft</dc:creator>
      <dc:date>2017-10-12T18:25:33Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703495#M43210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked your binary and can tell you the problem:&lt;/P&gt;&lt;P&gt;1. The Port and its interrupt (also in NVIC) is set up correctly.&lt;BR /&gt;2. The interrupt fires and its vector is taken, however you haven't installed the correct handler since it calls the "un-handled" interrupt which means that it hangs in the interrupt forever (with KDS you should have been able to see this too).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is easy to see that the vectors are missing (you have VTOR set to 0 - meaning that the vectors are hard-coded - you will probably find them in an assembler file somewhere).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the values that you have in Flash starting at address 0x00000000. I have labeled the vectors of interest, including the location of the "port B,C,D,E" interrupt vector (the last one).&lt;BR /&gt;Since the vector value is the same as many others it is clear that a un-handled (default) vector is being used rather than one to handle the port interrupt.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30062i7B49297ACF246C1A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;These are the values that you have in Flash starting at address 0x00000000. I have labeled the vectors of interest, including the location of the "port B,C,D,E" interrupt vector (the last one).&lt;BR /&gt;Since the vector value is the same as many others it is clear that a un-handled (default) vector is being used rather than one to handle the port interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you can work out why and where you need to add it you should be OK. You will however need to ensure that the handler used is suitable for a port interrupt shared by these 4 ports or, in the worst case, one that at least handles the port C case for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As noted before, if you would prefer a more power ful and fool-proof solution just down-load the (free) Open Source uTasker project since it handles all such details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 20:10:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703495#M43210</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-10-12T20:10:49Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703496#M43211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That solved the issue. In the board.h file was the IRQ Handler declared as "PORTBCDE_IRQHandler" for the Switch 3 but it should be "PORTB_PORTC_PORTD_PORTE_IRQHandler", like it is defined in the Vector Table in the file "startup_MKL27Z644.S". Now the Interrupt calls my IRQ handler-&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 22:39:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703496#M43211</guid>
      <dc:creator>killerawft</dc:creator>
      <dc:date>2017-10-12T22:39:49Z</dc:date>
    </item>
    <item>
      <title>Re: Freedom KL27 external GPIO Interrupt</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703497#M43212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P style="line-height: 23.8px; color: #000000; font-family: 'lucida Grande', Verdana, 'Microsoft YaHei'; font-size: 14px; font-style: normal; font-variant-ligatures: normal; font-variant-caps: normal; font-weight: normal; letter-spacing: normal; orphans: 2; text-align: start; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-stroke-width: 0px; background-color: #ffffff; text-decoration-style: initial; text-decoration-color: initial;"&gt;I am not sure if you have slove this problem.&lt;/P&gt;&lt;P style="line-height: 23.8px; color: #000000; font-family: 'lucida Grande', Verdana, 'Microsoft YaHei'; font-size: 14px; font-style: normal; font-variant-ligatures: normal; font-variant-caps: normal; font-weight: normal; letter-spacing: normal; orphans: 2; text-align: start; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-stroke-width: 0px; background-color: #ffffff; text-decoration-style: initial; text-decoration-color: initial;"&gt;You can refer the modification shown below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="PTC3 FRDM-KL27Z.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33417i85143B7AD305D39A/image-size/large?v=v2&amp;amp;px=999" role="button" title="PTC3 FRDM-KL27Z.png" alt="PTC3 FRDM-KL27Z.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'lucida Grande', Verdana, 'Microsoft YaHei'; font-size: 14px; font-style: normal; font-variant-ligatures: normal; font-variant-caps: normal; font-weight: normal; letter-spacing: normal; orphans: 2; text-align: start; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-stroke-width: 0px; background-color: #ffffff; text-decoration-style: initial; text-decoration-color: initial; display: inline !important; float: none;"&gt;Be notice that the PTC3 is connect to external signal through J18 by default.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: 'lucida Grande', Verdana, 'Microsoft YaHei'; font-size: 14px; font-style: normal; font-variant-ligatures: normal; font-variant-caps: normal; font-weight: normal; letter-spacing: normal; orphans: 2; text-align: start; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-stroke-width: 0px; background-color: #ffffff; text-decoration-style: initial; text-decoration-color: initial; display: inline !important; float: none;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="J28 PTC3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33376i3889E115F1FC7EF8/image-size/large?v=v2&amp;amp;px=999" role="button" title="J28 PTC3.png" alt="J28 PTC3.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Oct 2017 12:28:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Freedom-KL27-external-GPIO-Interrupt/m-p/703497#M43212</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-10-16T12:28:30Z</dc:date>
    </item>
  </channel>
</rss>