<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KEA-128 operation at 3.3v in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-128-operation-at-3-3v/m-p/702141#M43148</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello VIGNESH BALAJI,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1)Is it recommended to operate KEA-128 pins at 3.3 v instead of 5v?&lt;/P&gt;&lt;P&gt;Answer: Both 3.3V and 5 can work, because the KEA128 operation voltage is 2.7V to 5.5V.&lt;/P&gt;&lt;P&gt;2)What should i do to operate KEA-128 pins at 3.3 v?&lt;/P&gt;&lt;P&gt;Answer: Just power on the chip with 3.3V.&lt;/P&gt;&lt;P&gt;3)What are the consequences of operating KEA-128 pins at 3.3v?&lt;/P&gt;&lt;P&gt;Answer: No bad consequences, 3.3V is also the normal voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Aug 2017 03:21:22 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2017-08-22T03:21:22Z</dc:date>
    <item>
      <title>KEA-128 operation at 3.3v</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-128-operation-at-3-3v/m-p/702140#M43147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I want to operate the pins of KEA-128 at 3.3v instead of 5v, what are the things to do for it and consequences it has. I have the following questions based on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)Is it recommended to operate KEA-128 pins at 3.3 v instead of 5v?&lt;/P&gt;&lt;P&gt;2)What should i do to operate KEA-128 pins at 3.3 v?&lt;/P&gt;&lt;P&gt;3)What are the consequences of operating KEA-128 pins at 3.3v?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Aug 2017 04:56:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-128-operation-at-3-3v/m-p/702140#M43147</guid>
      <dc:creator>vigneshbalaji</dc:creator>
      <dc:date>2017-08-21T04:56:11Z</dc:date>
    </item>
    <item>
      <title>Re: KEA-128 operation at 3.3v</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-128-operation-at-3-3v/m-p/702141#M43148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello VIGNESH BALAJI,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1)Is it recommended to operate KEA-128 pins at 3.3 v instead of 5v?&lt;/P&gt;&lt;P&gt;Answer: Both 3.3V and 5 can work, because the KEA128 operation voltage is 2.7V to 5.5V.&lt;/P&gt;&lt;P&gt;2)What should i do to operate KEA-128 pins at 3.3 v?&lt;/P&gt;&lt;P&gt;Answer: Just power on the chip with 3.3V.&lt;/P&gt;&lt;P&gt;3)What are the consequences of operating KEA-128 pins at 3.3v?&lt;/P&gt;&lt;P&gt;Answer: No bad consequences, 3.3V is also the normal voltage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Aug 2017 03:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KEA-128-operation-at-3-3v/m-p/702141#M43148</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2017-08-22T03:21:22Z</dc:date>
    </item>
  </channel>
</rss>