<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KL28 clock distribution in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL28-clock-distribution/m-p/701505#M43126</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got the answer about question 1, please check below comments.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) FIRC clock source has auto-trim feature. How is SCG_FIRCTCFG_TRIMDIV supposed to be set when SOSC is used as trim reference?&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;TS: The FIRC pre-divider is intended for the SOSC and the expectation is to set the div ratio to give&amp;nbsp; a 31250khz divided clock.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Sep 2017 06:24:01 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2017-09-20T06:24:01Z</dc:date>
    <item>
      <title>KL28 clock distribution</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL28-clock-distribution/m-p/701503#M43124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've got some questions regarding KL28 clock distribution subsystem. Please, can someone clarify the following?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) FIRC clock source has auto-trim feature. How is SCG_FIRCTCFG_TRIMDIV supposed to be set when SOSC is used as trim reference?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.) RTC_CR contains SCxP load capacitor configuration bits and OSCE for oscillator control. SCG contains similar fields (SCG_SOSCCFG_SCxP and SCG_SOSCCSR_SOSCEN). How are RTC and SCG oscillator settings related?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.) SCG_SOSCCSR contains SOSCERCLKEN bit that is described as "System OSC 3V ERCLK Enable" in refman rev. 4. What does "3V" means? Is this the same clock tree as ERCLK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 12:19:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL28-clock-distribution/m-p/701503#M43124</guid>
      <dc:creator>mst_</dc:creator>
      <dc:date>2017-09-12T12:19:42Z</dc:date>
    </item>
    <item>
      <title>Re: KL28 clock distribution</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL28-clock-distribution/m-p/701504#M43125</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1&amp;gt; I am checking with Kinetis product team to get the question 1 answer. I will let you know later;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2&amp;gt; The SCG module provides the system crystal oscillator, the SCG_SOSCCFG_SCxP and SCG_SOSCCSR_SOSCEN registers bits used to control the system crystal oscillator.&lt;BR /&gt;The RTC module register doesn't have related 32KHz oscillator, the related capacitor load bit has no function. The RTC used OSC32KCLK is from SCG output from the SOSC.&lt;/P&gt;&lt;P&gt;More detailed info, please check KL28 reference manual chapter 5.8.1 OSC32KCLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3&amp;gt; It is the same clock source of SCG ERCLK (clock from EXTAL0 pin). The 3V means the KL28 system OSC is 3V chip, which doesn't support 5V clock input.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29496i3635EB8CA440AA62/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Sep 2017 08:14:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL28-clock-distribution/m-p/701504#M43125</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-09-18T08:14:43Z</dc:date>
    </item>
    <item>
      <title>Re: KL28 clock distribution</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL28-clock-distribution/m-p/701505#M43126</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got the answer about question 1, please check below comments.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) FIRC clock source has auto-trim feature. How is SCG_FIRCTCFG_TRIMDIV supposed to be set when SOSC is used as trim reference?&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;TS: The FIRC pre-divider is intended for the SOSC and the expectation is to set the div ratio to give&amp;nbsp; a 31250khz divided clock.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Sep 2017 06:24:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL28-clock-distribution/m-p/701505#M43126</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-09-20T06:24:01Z</dc:date>
    </item>
  </channel>
</rss>