<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックPin sharing between ADC channel and KBI</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-sharing-between-ADC-channel-and-KBI/m-p/701229#M43122</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a S9KEAZN custom board and I would like to know if I can pin share between two peripheral ADC and KBI. I try adding an extra channel in my ADC but unfortunately I am using the same pin as a KBI for waking up and putting the CPU to sleep. Is there a way I can use the same pin in two different peripherals?&lt;/P&gt;&lt;P&gt;Also when I try doing this, the PE component ADC throws an error stating that I cannot add a channel since the pin is already used by KBI. Is there a work around for this. I am not too enthused about redesigning&amp;nbsp;on the hardware.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Sep 2017 15:48:31 GMT</pubDate>
    <dc:creator>saipriyasubrama</dc:creator>
    <dc:date>2017-09-12T15:48:31Z</dc:date>
    <item>
      <title>Pin sharing between ADC channel and KBI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-sharing-between-ADC-channel-and-KBI/m-p/701229#M43122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a S9KEAZN custom board and I would like to know if I can pin share between two peripheral ADC and KBI. I try adding an extra channel in my ADC but unfortunately I am using the same pin as a KBI for waking up and putting the CPU to sleep. Is there a way I can use the same pin in two different peripherals?&lt;/P&gt;&lt;P&gt;Also when I try doing this, the PE component ADC throws an error stating that I cannot add a channel since the pin is already used by KBI. Is there a work around for this. I am not too enthused about redesigning&amp;nbsp;on the hardware.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 15:48:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-sharing-between-ADC-channel-and-KBI/m-p/701229#M43122</guid>
      <dc:creator>saipriyasubrama</dc:creator>
      <dc:date>2017-09-12T15:48:31Z</dc:date>
    </item>
    <item>
      <title>Re: Pin sharing between ADC channel and KBI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-sharing-between-ADC-channel-and-KBI/m-p/701230#M43123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi SAIPRIYA,&lt;/P&gt;&lt;P&gt;I'm not very clear of your applictaion. Some time we share the pin between digital functions, but it's rarely share between digital and analog functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Sep 2017 08:16:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Pin-sharing-between-ADC-channel-and-KBI/m-p/701230#M43123</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2017-09-13T08:16:25Z</dc:date>
    </item>
  </channel>
</rss>