<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can I program a MKL15Z128VFM4 firmware file without modifications on MKL16Z128VFM4 part? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-program-a-MKL15Z128VFM4-firmware-file-without/m-p/700429#M43062</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are having issues buying the MKL15Z128VFM4 part from distributors as they are out of stock. The&amp;nbsp;MKL16Z128VFM4 and MKL17Z128VFM4 parts are, however, available (the first may be bought directly from NXP buy-direct).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I already know the parts are compatible, but I am not sure on what level!&lt;/P&gt;&lt;P&gt;As I may update some existent devices directly in field, I don't want to manage multiple firmware versions&amp;nbsp;- so having the same firmware for both parts is desired.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The main question is: may I program the same firmware (I mean, the same .srec/hex file) I used on MKL15 based devices on the MKL16 new ones? Or do I need to generate a new one and manage two versions of the firmware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Important: I'm not using i2s in my design (I've already seen this is a new feature on MKL16)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much! I appreciate your help as our product is almost on back order!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Sep 2017 20:22:24 GMT</pubDate>
    <dc:creator>lfschrickte</dc:creator>
    <dc:date>2017-09-11T20:22:24Z</dc:date>
    <item>
      <title>Can I program a MKL15Z128VFM4 firmware file without modifications on MKL16Z128VFM4 part?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-program-a-MKL15Z128VFM4-firmware-file-without/m-p/700429#M43062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are having issues buying the MKL15Z128VFM4 part from distributors as they are out of stock. The&amp;nbsp;MKL16Z128VFM4 and MKL17Z128VFM4 parts are, however, available (the first may be bought directly from NXP buy-direct).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I already know the parts are compatible, but I am not sure on what level!&lt;/P&gt;&lt;P&gt;As I may update some existent devices directly in field, I don't want to manage multiple firmware versions&amp;nbsp;- so having the same firmware for both parts is desired.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The main question is: may I program the same firmware (I mean, the same .srec/hex file) I used on MKL15 based devices on the MKL16 new ones? Or do I need to generate a new one and manage two versions of the firmware?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Important: I'm not using i2s in my design (I've already seen this is a new feature on MKL16)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much! I appreciate your help as our product is almost on back order!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Sep 2017 20:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-program-a-MKL15Z128VFM4-firmware-file-without/m-p/700429#M43062</guid>
      <dc:creator>lfschrickte</dc:creator>
      <dc:date>2017-09-11T20:22:24Z</dc:date>
    </item>
    <item>
      <title>Re: Can I program a MKL15Z128VFM4 firmware file without modifications on MKL16Z128VFM4 part?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-program-a-MKL15Z128VFM4-firmware-file-without/m-p/700430#M43063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luiz Fernando Schrickte&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Answering your question, yes, you can load the same .bin in the two devices as long as these two parts are compatibles and form the same family.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you mentioned, you will have to pay attention the new modules that are included in the MKL16, you mentioned I2S, but please also consider that the SPI is 16-bit SPI modules in the kl16, while 8 bit in the kl15. Also, there could be some some pins that you have available in the kl16 that are not in the kl15, I recommend you to check the pinout.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this could help.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Sep 2017 01:53:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-program-a-MKL15Z128VFM4-firmware-file-without/m-p/700430#M43063</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-09-14T01:53:03Z</dc:date>
    </item>
    <item>
      <title>Re: Can I program a MKL15Z128VFM4 firmware file without modifications on MKL16Z128VFM4 part?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-program-a-MKL15Z128VFM4-firmware-file-without/m-p/700431#M43064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As our stock is getting low right now I definitely had to port the firmware!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I needed to change the firmware for the MKL16 as the MKL15 compiled bin file didn't work directly. After changing the Cpu through PE,&amp;nbsp; I noticed there are slight differentes at SM1.c:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot from 2017-12-15 17-05-34.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27354iBD947B883DA5AA58/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2017-12-15 17-05-34.png" alt="Screenshot from 2017-12-15 17-05-34.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously trying to run the MKL16 firmware on MKL15 doesn't work either. I am now working on a firmware that should be compatible with both (checking SUBFAMID on SDID), as I have field update features.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The big question now is: it looks like I am late again, as the MKL16 part is rare now among suppliers (wans't at the time of the first question). NXP informed me their lead time is around 39 weeks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am thinking to port to MKL17 (as this subfamily has parts available). It looks like there is no PE support, so I'll need to port it all by myself - the big question is: what changed? Do Freescale has a single/organized source of changes in this subfamilies upgrades? Or are they not meant to be successors, but new family members? Does somebody know what changes I will need to make in the software?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you again!&lt;/P&gt;&lt;P&gt;Luiz Fernando&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Dec 2017 19:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-I-program-a-MKL15Z128VFM4-firmware-file-without/m-p/700431#M43064</guid>
      <dc:creator>lfschrickte</dc:creator>
      <dc:date>2017-12-15T19:29:56Z</dc:date>
    </item>
  </channel>
</rss>