<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MK12DN512VLK5 - Contradictory flash clock divider requirements</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DN512VLK5-Contradictory-flash-clock-divider-requirements/m-p/700167#M43048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom scott&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the misunderstanding description in the reference manual, the note in the page 134 should be like &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The flash clock frequency must be programmed to 25 MHz or less, less than or equal to the bus clock, and an integer divide of the core clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you cannot have&lt;/P&gt;&lt;P&gt;48 MHz core/system&lt;/P&gt;&lt;P&gt;8 MHz bus&lt;/P&gt;&lt;P&gt;24 MHz flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information could help you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Sep 2017 00:41:21 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2017-09-12T00:41:21Z</dc:date>
    <item>
      <title>MK12DN512VLK5 - Contradictory flash clock divider requirements</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DN512VLK5-Contradictory-flash-clock-divider-requirements/m-p/700166#M43047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Reference Manual:&amp;nbsp;K12P80M50SF4RM, Rev 4, Feb 2013&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Page 134, Section 5.5: "The flash clock frequency must be programmed to 25 MHz or less and an integer&lt;BR /&gt;divide of the bus clock."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Page 233, Section 12.2.11 - System Clock Divider Register 1 (SIM_CLKDIV1):&lt;/P&gt;&lt;P&gt;OUTDIV4 - "The flash clock frequency must be an integer divide of the system clock frequency."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to set the clocks up as follows:&lt;/P&gt;&lt;P&gt;48 MHz core/system&lt;/P&gt;&lt;P&gt;8 MHz bus&lt;/P&gt;&lt;P&gt;24 MHz flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can do this following the requirement on page 233, but not the requirement on page 134.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which requirement is correct?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Sep 2017 16:23:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DN512VLK5-Contradictory-flash-clock-divider-requirements/m-p/700166#M43047</guid>
      <dc:creator>tomscott</dc:creator>
      <dc:date>2017-09-11T16:23:57Z</dc:date>
    </item>
    <item>
      <title>Re: MK12DN512VLK5 - Contradictory flash clock divider requirements</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DN512VLK5-Contradictory-flash-clock-divider-requirements/m-p/700167#M43048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom scott&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the misunderstanding description in the reference manual, the note in the page 134 should be like &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The flash clock frequency must be programmed to 25 MHz or less, less than or equal to the bus clock, and an integer divide of the core clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you cannot have&lt;/P&gt;&lt;P&gt;48 MHz core/system&lt;/P&gt;&lt;P&gt;8 MHz bus&lt;/P&gt;&lt;P&gt;24 MHz flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information could help you.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Sep 2017 00:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK12DN512VLK5-Contradictory-flash-clock-divider-requirements/m-p/700167#M43048</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-09-12T00:41:21Z</dc:date>
    </item>
  </channel>
</rss>