<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: What is max interrupt frequency for K30</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-max-interrupt-frequency-for-K30/m-p/699925#M43028</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Burak,&lt;/P&gt;&lt;P&gt;K30 PIT clock source is the BUS clock which can be set to the max value 50M. And there is no restriction for PITx_LDVALn. So it can generate interrupt in a very high frequency.&lt;/P&gt;&lt;P&gt;The only problem of high interrupt frequency is whether the MCU has enough time to deal with so much interrupt. If not, interrupt will be pending and then lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Sep 2017 07:34:02 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2017-09-13T07:34:02Z</dc:date>
    <item>
      <title>What is max interrupt frequency for K30</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-max-interrupt-frequency-for-K30/m-p/699924#M43027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For Exp: Can K30 handle about 200kHz(other hand every 5us) PIT interrupt?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Sep 2017 07:58:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-max-interrupt-frequency-for-K30/m-p/699924#M43027</guid>
      <dc:creator>burakduzgun</dc:creator>
      <dc:date>2017-09-11T07:58:08Z</dc:date>
    </item>
    <item>
      <title>Re: What is max interrupt frequency for K30</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-max-interrupt-frequency-for-K30/m-p/699925#M43028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Burak,&lt;/P&gt;&lt;P&gt;K30 PIT clock source is the BUS clock which can be set to the max value 50M. And there is no restriction for PITx_LDVALn. So it can generate interrupt in a very high frequency.&lt;/P&gt;&lt;P&gt;The only problem of high interrupt frequency is whether the MCU has enough time to deal with so much interrupt. If not, interrupt will be pending and then lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Sep 2017 07:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-max-interrupt-frequency-for-K30/m-p/699925#M43028</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2017-09-13T07:34:02Z</dc:date>
    </item>
    <item>
      <title>Re: What is max interrupt frequency for K30</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-max-interrupt-frequency-for-K30/m-p/699926#M43029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So thus assuming a 100MHz core-clock, 5us encompasses 500 instruction cycles.&amp;nbsp; ASSUMING a 'couple dozen' clocks are consumed by interrupt hardware processes, that still leaves a 'fair number' of clocks for a 'lean' interrupt handler and 'leftovers' for the rest of the work to be done...&amp;nbsp;&amp;nbsp; 200KHz is certainly 'not unreasonable' to handle.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Sep 2017 11:38:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-max-interrupt-frequency-for-K30/m-p/699926#M43029</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2017-09-13T11:38:02Z</dc:date>
    </item>
    <item>
      <title>Re: What is max interrupt frequency for K30</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-max-interrupt-frequency-for-K30/m-p/699927#M43030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for reply&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 07:12:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-is-max-interrupt-frequency-for-K30/m-p/699927#M43030</guid>
      <dc:creator>burakduzgun</dc:creator>
      <dc:date>2018-02-22T07:12:18Z</dc:date>
    </item>
  </channel>
</rss>