<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MRB-KW019032NA interface to Raspberry Pi in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MRB-KW019032NA-interface-to-Raspberry-Pi/m-p/699464#M43010</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a MRB-KW019032NA and am trying to connect to my Raspberry Pi through UART interface. It is supposed to receive signals from a&amp;nbsp;FXTH870511 TPMS sensor and pass them over to Pi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MRB-Kw01 manual it says how it could be mounted on a TWR-RF board and how jumper setting should change (relative to the standalone case). Now I would like to do the same thing with Raspberry Pi instead of TWR-RF and I wonder if anybody here has experience to help me. Thanks alot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Aug 2017 18:21:44 GMT</pubDate>
    <dc:creator>aliasgharrajabi</dc:creator>
    <dc:date>2017-08-16T18:21:44Z</dc:date>
    <item>
      <title>MRB-KW019032NA interface to Raspberry Pi</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MRB-KW019032NA-interface-to-Raspberry-Pi/m-p/699464#M43010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a MRB-KW019032NA and am trying to connect to my Raspberry Pi through UART interface. It is supposed to receive signals from a&amp;nbsp;FXTH870511 TPMS sensor and pass them over to Pi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MRB-Kw01 manual it says how it could be mounted on a TWR-RF board and how jumper setting should change (relative to the standalone case). Now I would like to do the same thing with Raspberry Pi instead of TWR-RF and I wonder if anybody here has experience to help me. Thanks alot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Aug 2017 18:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MRB-KW019032NA-interface-to-Raspberry-Pi/m-p/699464#M43010</guid>
      <dc:creator>aliasgharrajabi</dc:creator>
      <dc:date>2017-08-16T18:21:44Z</dc:date>
    </item>
    <item>
      <title>Re: MRB-KW019032NA interface to Raspberry Pi</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MRB-KW019032NA-interface-to-Raspberry-Pi/m-p/699465#M43011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Aliasghar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can take a look at the &lt;A href="http://www.nxp.com/downloads/en/printed-circuit-boards-reference-designs/KW01-MRB_PCBRD.zip"&gt;MRB-KW0x Schematic&lt;/A&gt;&amp;nbsp;and the TWR-RF schematic in the&amp;nbsp;&lt;A href="http://www.nxp.com/docs/en/reference-manual/TWRRFRM.pdf"&gt;TWR-RF Module Reference Manual&lt;/A&gt;&amp;nbsp;to see how the connections are being made between both boards. From the MRB-KW0x board headers you should be able to get access to the UART signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Aug 2017 21:35:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MRB-KW019032NA-interface-to-Raspberry-Pi/m-p/699465#M43011</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2017-08-28T21:35:47Z</dc:date>
    </item>
  </channel>
</rss>