<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flashing MKW30Z over SWD in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-MKW30Z-over-SWD/m-p/696664#M42853</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to program MKW30Z via SWD, using another ARM chip's GPIO. It would be really helpful to see an example sequence for loading firmware to the chip, similar to the below code on github for EFM32. Is there&amp;nbsp; something like that in SDK, or may be in some open source project(s)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/disk91/PySWD/blob/master/EFM32.py" title="https://github.com/disk91/PySWD/blob/master/EFM32.py"&gt;PySWD/EFM32.py at master · disk91/PySWD · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Aug 2017 11:26:08 GMT</pubDate>
    <dc:creator>ivandrobyshevs1</dc:creator>
    <dc:date>2017-08-11T11:26:08Z</dc:date>
    <item>
      <title>Flashing MKW30Z over SWD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-MKW30Z-over-SWD/m-p/696664#M42853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to program MKW30Z via SWD, using another ARM chip's GPIO. It would be really helpful to see an example sequence for loading firmware to the chip, similar to the below code on github for EFM32. Is there&amp;nbsp; something like that in SDK, or may be in some open source project(s)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://github.com/disk91/PySWD/blob/master/EFM32.py" title="https://github.com/disk91/PySWD/blob/master/EFM32.py"&gt;PySWD/EFM32.py at master · disk91/PySWD · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Aug 2017 11:26:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-MKW30Z-over-SWD/m-p/696664#M42853</guid>
      <dc:creator>ivandrobyshevs1</dc:creator>
      <dc:date>2017-08-11T11:26:08Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing MKW30Z over SWD</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-MKW30Z-over-SWD/m-p/696665#M42854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Turned out that recent OpenOCD supports KW30Z, and I was able to program it that way.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Aug 2017 15:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flashing-MKW30Z-over-SWD/m-p/696665#M42854</guid>
      <dc:creator>ivandrobyshevs1</dc:creator>
      <dc:date>2017-08-22T15:04:15Z</dc:date>
    </item>
  </channel>
</rss>