<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S25fl512s flash not working with spi in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S25fl512s-flash-not-working-with-spi/m-p/693836#M42750</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on interfacing a spi flash module s25fl512s with MK64FN1M0vll12 controller.&lt;/P&gt;&lt;P&gt;Using processor expert and ksdk 1.3 I generated the Dspi module for spi 1. Disabled the chip select.&lt;/P&gt;&lt;P&gt;Used gpio pin as chip select .&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to get the clock running and also shows the data on SDO pin of microcontroller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I am not getting any response from the flash. It giving it as 0's when trying to read identification using RDID command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried spi in both modes , mode 0 and mode 1, but no success. I tried spi with different speeds with maximum of 1 Mhz.&lt;/P&gt;&lt;P&gt;Any help will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sanket&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 May 2017 11:53:48 GMT</pubDate>
    <dc:creator>ksk10</dc:creator>
    <dc:date>2017-05-26T11:53:48Z</dc:date>
    <item>
      <title>S25fl512s flash not working with spi</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S25fl512s-flash-not-working-with-spi/m-p/693836#M42750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on interfacing a spi flash module s25fl512s with MK64FN1M0vll12 controller.&lt;/P&gt;&lt;P&gt;Using processor expert and ksdk 1.3 I generated the Dspi module for spi 1. Disabled the chip select.&lt;/P&gt;&lt;P&gt;Used gpio pin as chip select .&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to get the clock running and also shows the data on SDO pin of microcontroller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I am not getting any response from the flash. It giving it as 0's when trying to read identification using RDID command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried spi in both modes , mode 0 and mode 1, but no success. I tried spi with different speeds with maximum of 1 Mhz.&lt;/P&gt;&lt;P&gt;Any help will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sanket&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 May 2017 11:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S25fl512s-flash-not-working-with-spi/m-p/693836#M42750</guid>
      <dc:creator>ksk10</dc:creator>
      <dc:date>2017-05-26T11:53:48Z</dc:date>
    </item>
    <item>
      <title>Re: S25fl512s flash not working with spi</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/S25fl512s-flash-not-working-with-spi/m-p/693837#M42751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Sanket&lt;/P&gt;&lt;P&gt;can you list the code to access spi flash? can you paste the scope screenshot of spi signals: SCK/MOSI/MISO/SS?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 10:02:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/S25fl512s-flash-not-working-with-spi/m-p/693837#M42751</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-06-01T10:02:22Z</dc:date>
    </item>
  </channel>
</rss>