<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックLow-speed USB operation in host mode on the K22?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-speed-USB-operation-in-host-mode-on-the-K22/m-p/693765#M42744</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm pretty sure the answer to this ought to be 'yes', but I don't see it clearly documented and I want to check before I waste too much time on a dead end. &amp;nbsp;Does the K22 series support low speed USB (not full speed) in host mode? &amp;nbsp;I'm thinking about interfacing a specialty device that only supports low speed mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second half of my question is what USB stack should I be using for a new project? &amp;nbsp;One in KSDK 2, I assume? &amp;nbsp;I'm still on the now-obsolete 4.x bare metal stack for my current projects.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Aug 2017 05:17:30 GMT</pubDate>
    <dc:creator>scottm</dc:creator>
    <dc:date>2017-08-04T05:17:30Z</dc:date>
    <item>
      <title>Low-speed USB operation in host mode on the K22?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-speed-USB-operation-in-host-mode-on-the-K22/m-p/693765#M42744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm pretty sure the answer to this ought to be 'yes', but I don't see it clearly documented and I want to check before I waste too much time on a dead end. &amp;nbsp;Does the K22 series support low speed USB (not full speed) in host mode? &amp;nbsp;I'm thinking about interfacing a specialty device that only supports low speed mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The second half of my question is what USB stack should I be using for a new project? &amp;nbsp;One in KSDK 2, I assume? &amp;nbsp;I'm still on the now-obsolete 4.x bare metal stack for my current projects.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Aug 2017 05:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-speed-USB-operation-in-host-mode-on-the-K22/m-p/693765#M42744</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2017-08-04T05:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: Low-speed USB operation in host mode on the K22?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-speed-USB-operation-in-host-mode-on-the-K22/m-p/693766#M42745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;Yes, you are correct. The USB module of K22 operates at Full Speed. &lt;BR /&gt;The Low Speed support is for when it operates as Host and LS devices are connected to it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;Low speed devices use pull-up resistor on D- line. So you will need to disable the D+ resistor and add externally a pull-up resistor on D-.&lt;BR /&gt; (Because OTG controller does not have a field to enable pull-up resistor on D-)&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif;"&gt;For software change, remember that maximum packet size must be set according low speed specifications.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 06:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-speed-USB-operation-in-host-mode-on-the-K22/m-p/693766#M42745</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-08-09T06:08:35Z</dc:date>
    </item>
    <item>
      <title>Re: Low-speed USB operation in host mode on the K22?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-speed-USB-operation-in-host-mode-on-the-K22/m-p/693767#M42746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's exactly what I was looking for, thank you very much! &amp;nbsp;Now to see if anyone has written any MIDI code for this thing...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Scott&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 16:17:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Low-speed-USB-operation-in-host-mode-on-the-K22/m-p/693767#M42746</guid>
      <dc:creator>scottm</dc:creator>
      <dc:date>2017-08-09T16:17:13Z</dc:date>
    </item>
  </channel>
</rss>