<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK70 LCDC H_WIDTH settings</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-H-WIDTH-settings/m-p/693295#M42702</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have downloaded the source files for the K70 lcdc example and modified the code for a 800x600 TFT LCD panel. The timings have an hsync pulse width of 128, but since the LCDC_LHCR only has 6 bits available for the H_WIDTH settings, the 128 value is not possible. I am getting scrolling horizontal lines on the left side of my panel that also flicker. Are we setting up the registers correctly? I've attached the datasheet for the panel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Sally&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Aug 2017 15:10:52 GMT</pubDate>
    <dc:creator>sallys</dc:creator>
    <dc:date>2017-08-03T15:10:52Z</dc:date>
    <item>
      <title>K70 LCDC H_WIDTH settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-H-WIDTH-settings/m-p/693295#M42702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have downloaded the source files for the K70 lcdc example and modified the code for a 800x600 TFT LCD panel. The timings have an hsync pulse width of 128, but since the LCDC_LHCR only has 6 bits available for the H_WIDTH settings, the 128 value is not possible. I am getting scrolling horizontal lines on the left side of my panel that also flicker. Are we setting up the registers correctly? I've attached the datasheet for the panel.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Sally&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2017 15:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-H-WIDTH-settings/m-p/693295#M42702</guid>
      <dc:creator>sallys</dc:creator>
      <dc:date>2017-08-03T15:10:52Z</dc:date>
    </item>
    <item>
      <title>Re: K70 LCDC H_WIDTH settings</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-H-WIDTH-settings/m-p/693296#M42703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sally,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the LQ121S1LG81 SPEC, the Hsync pluse width typical value is 128 clock, while the Min. value is 2. I think the K70 LCDC_LHCR register set [H_WIDTH] to 0x3F should be working.&lt;/P&gt;&lt;P&gt;The LQ121S1LG81&amp;nbsp; LCD clock frequency is in range of [35~42]MHz, how about the K70 LCDC clock setting?&lt;/P&gt;&lt;P&gt;If the LSCLK clock frequency is in range of LQ121S1LG81 spec required?&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Aug 2017 05:45:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-LCDC-H-WIDTH-settings/m-p/693296#M42703</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-08-08T05:45:07Z</dc:date>
    </item>
  </channel>
</rss>