<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KL03 write to flash in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689494#M42449</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been using the Forth Language for nearly 40 years on many, many &lt;/P&gt;&lt;P&gt;projects, big and small.  It's never let me down.&lt;/P&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Fully interactive, like BASIC but hugely more sophisticated  NO &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;BREAKPOINTS NEEDED&lt;/P&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;No linker&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Easier to read than C code&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Built-in multi-tasker&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Built-in Assembler&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;EXTREMELY compact code*&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Same language and operating system across numerous targets, all &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;from a single vendor&lt;/P&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Can extend the cross-compiler as needed.  This is quite easy &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;and can be hugely useful in writing readable code.&lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;I once wrote the code for a PLC including its application on a 6801 &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;single chipper, residing in just 4KB.  How about that for compact?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.forth.com/" target="test_blank"&gt;https://www.forth.com/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Concerning my future project...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The original version used the ATmega168&lt;/P&gt;&lt;P&gt;Then another variant the ATtiny1634&lt;/P&gt;&lt;P&gt;I was going to use an ATtiny84A on the next one, until I discovered the KL03&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've just done 2 projects on the SilLabs M0+ and fallen in love with 32bits&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;all of these are in Forth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tone&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Aug 2017 04:54:40 GMT</pubDate>
    <dc:creator>tonyware</dc:creator>
    <dc:date>2017-08-01T04:54:40Z</dc:date>
    <item>
      <title>KL03 write to flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689490#M42445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can I write some code in the KL03 to allow it to write a parameter into its flash?&amp;nbsp; Paramater write tot needed very often, but read frequently&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2017 14:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689490#M42445</guid>
      <dc:creator>tonyware</dc:creator>
      <dc:date>2017-07-31T14:45:46Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 write to flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689491#M42446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Flash parameters are possible with the KL03 as with any other Kinetis part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;See &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis%2FFRDM-KL03Z.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis/FRDM-KL03Z.html&lt;/A&gt;&lt;BR /&gt;At the bottom of that page there is a &lt;STRONG&gt;binary&lt;/STRONG&gt; that you can try and also a link to a &lt;STRONG&gt;video explaining the operation&lt;/STRONG&gt;. All code, including a number of different parameter system options, is available in the uTasker project (allows also simulation of the KL03 and its internal Flash operation).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2017 17:39:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689491#M42446</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-07-31T17:39:17Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 write to flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689492#M42447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nice little chip, price is about right in volume too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm going to use the KL03 using Forth Inc's SwiftX cross compiler &lt;/P&gt;&lt;P&gt;system and Segger Jlink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tone&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2017 18:06:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689492#M42447</guid>
      <dc:creator>tonyware</dc:creator>
      <dc:date>2017-07-31T18:06:03Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 write to flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689493#M42448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have never used SwiftX cross compiler (and IDE).&lt;BR /&gt;What is the advantages compared to the cross compilers and IDEs that are commonly used for Kinetis developments [MCUXpresso, KDS, CW10.x, S32, Atollic, IAR, Keil, Rowley, Green Hills, CooCox etc.] ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2017 21:47:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689493#M42448</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-07-31T21:47:21Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 write to flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689494#M42449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've been using the Forth Language for nearly 40 years on many, many &lt;/P&gt;&lt;P&gt;projects, big and small.  It's never let me down.&lt;/P&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Fully interactive, like BASIC but hugely more sophisticated  NO &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;BREAKPOINTS NEEDED&lt;/P&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;No linker&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Easier to read than C code&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Built-in multi-tasker&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Built-in Assembler&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;EXTREMELY compact code*&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Same language and operating system across numerous targets, all &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;from a single vendor&lt;/P&gt;&lt;P&gt;    &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;Can extend the cross-compiler as needed.  This is quite easy &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;and can be hugely useful in writing readable code.&lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;I once wrote the code for a PLC including its application on a 6801 &lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;single chipper, residing in just 4KB.  How about that for compact?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.forth.com/" target="test_blank"&gt;https://www.forth.com/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Concerning my future project...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The original version used the ATmega168&lt;/P&gt;&lt;P&gt;Then another variant the ATtiny1634&lt;/P&gt;&lt;P&gt;I was going to use an ATtiny84A on the next one, until I discovered the KL03&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've just done 2 projects on the SilLabs M0+ and fallen in love with 32bits&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;all of these are in Forth&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tone&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 04:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689494#M42449</guid>
      <dc:creator>tonyware</dc:creator>
      <dc:date>2017-08-01T04:54:40Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 write to flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689495#M42450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the information. I have heard from others about how good Forth can be but I never used it myself. Also I have never had a customer who used it (or requested it) so I suppose that is why I have also stuck with C. I wonder whether there are any Kinetis peripheral libraries in Forth? (Or TCP/IP stacks and USB libraries suitable for Kinetis parts).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 15:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689495#M42450</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-08-01T15:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 write to flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689496#M42451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a read of this in 'your copious free time' (!!!)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tone&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 21:27:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-write-to-flash/m-p/689496#M42451</guid>
      <dc:creator>tonyware</dc:creator>
      <dc:date>2017-08-01T21:27:27Z</dc:date>
    </item>
  </channel>
</rss>