<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Hexiwear K64 Externel reference clock in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hexiwear-K64-Externel-reference-clock/m-p/689160#M42413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to select external oscillator (12MHz) as MCGOUTCLK but the status bit in MCG_S showing selection of external clock does not set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have enabled clock for PORTA, OSCSEL is 0 to select OSC0. RANGE is selected as 1 and CLKS as 2.&lt;/P&gt;&lt;P&gt;After that IREFST bit in MCG_S is not cleared and also CLKST bits remain to show internal clock selection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have consulted source code for hexiwear firmware and bootloader. I cannot find any other settings.&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jun 2017 09:21:32 GMT</pubDate>
    <dc:creator>amnatehreem</dc:creator>
    <dc:date>2017-06-16T09:21:32Z</dc:date>
    <item>
      <title>Hexiwear K64 Externel reference clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hexiwear-K64-Externel-reference-clock/m-p/689160#M42413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to select external oscillator (12MHz) as MCGOUTCLK but the status bit in MCG_S showing selection of external clock does not set.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have enabled clock for PORTA, OSCSEL is 0 to select OSC0. RANGE is selected as 1 and CLKS as 2.&lt;/P&gt;&lt;P&gt;After that IREFST bit in MCG_S is not cleared and also CLKST bits remain to show internal clock selection.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have consulted source code for hexiwear firmware and bootloader. I cannot find any other settings.&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jun 2017 09:21:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hexiwear-K64-Externel-reference-clock/m-p/689160#M42413</guid>
      <dc:creator>amnatehreem</dc:creator>
      <dc:date>2017-06-16T09:21:32Z</dc:date>
    </item>
    <item>
      <title>Re: Hexiwear K64 Externel reference clock</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hexiwear-K64-Externel-reference-clock/m-p/689161#M42414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the CodeWarrior IDE software embedded [Processor Expert] tool generated the MCG initialization code for your reference (using external 12MHz crystal and MCG working at PEE mode with core clock 120MHz &amp;amp; bus clock 60MHz):&lt;/P&gt;&lt;P&gt;More detailed info, please refer attached &amp;lt;CPU_Init.c&amp;gt; &amp;amp; &amp;lt;CPU_Config.h&amp;gt; files.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jun 2017 06:48:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Hexiwear-K64-Externel-reference-clock/m-p/689161#M42414</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-06-19T06:48:46Z</dc:date>
    </item>
  </channel>
</rss>