<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-K22F in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F/m-p/688660#M42372</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jose,&lt;/P&gt;&lt;P&gt;Please download the SDK_2.2_FRDM-K22F package refer &lt;A _jive_internal="true" data-containerid="11554" data-containertype="14" data-objectid="333304" data-objecttype="102" href="https://community.nxp.com/docs/DOC-333304"&gt;Generating a downloadable MCUXpresso SDK v.2 package&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Then you can modify the led_output example to toggle the Green LED.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25113i389E269D585F6212/image-size/large?v=v2&amp;amp;px=999" title="led_output.png" alt="led_output.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25292i71019288DE76AAD9/image-size/large?v=v2&amp;amp;px=999" title="led_output SDK_2.2_FRDM-K22F.png" alt="led_output SDK_2.2_FRDM-K22F.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jul 2017 01:20:39 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2017-07-12T01:20:39Z</dc:date>
    <item>
      <title>FRDM-K22F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F/m-p/688659#M42371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I have just bought a FRDM-K22F, I am using the openSDA connector to debug my code, when I download my application to debug it, I can see the D2 LED flashing but at the same time the RGB led is switch on in GREEN without running the code, then I can´t switching off in anyway.&lt;/P&gt;&lt;P&gt;Someone can advise me why that it could be possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Jul 2017 17:50:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F/m-p/688659#M42371</guid>
      <dc:creator>josemartinez</dc:creator>
      <dc:date>2017-07-09T17:50:48Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K22F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F/m-p/688660#M42372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jose,&lt;/P&gt;&lt;P&gt;Please download the SDK_2.2_FRDM-K22F package refer &lt;A _jive_internal="true" data-containerid="11554" data-containertype="14" data-objectid="333304" data-objecttype="102" href="https://community.nxp.com/docs/DOC-333304"&gt;Generating a downloadable MCUXpresso SDK v.2 package&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Then you can modify the led_output example to toggle the Green LED.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25113i389E269D585F6212/image-size/large?v=v2&amp;amp;px=999" title="led_output.png" alt="led_output.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25292i71019288DE76AAD9/image-size/large?v=v2&amp;amp;px=999" title="led_output SDK_2.2_FRDM-K22F.png" alt="led_output SDK_2.2_FRDM-K22F.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2017 01:20:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K22F/m-p/688660#M42372</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2017-07-12T01:20:39Z</dc:date>
    </item>
  </channel>
</rss>