<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Mount 2 MSD with FATfs</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mount-2-MSD-with-FATfs/m-p/687134#M42300</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aniket Markande&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, if you are using the latest USB stack (the one that comes with SDK2.x), it already support HUB drivers. You can find in usb_host_config.h file a macro definitions as #define USB_HOST_CONFIG_HUB (1U), this will enable Host HUB class driver is enable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regardless of this, the given example doesn't implement the support for more MSD, but you can add it to it:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. You have to add a new mass storage device instance, the example uses the g_MsdFatfsInstance global variable for the instance, so you could add a g_MsdFatfsInstance_2.&lt;/P&gt;&lt;P&gt;2. Inside app.c you can see that this instance is used to create the task with USB_HostMsdTask(&amp;amp;g_MsdFatfsInstance); (this variable is declared here as extern because we actually used in host_msd_fatfs.c).&lt;/P&gt;&lt;P&gt;3. In host_msd_fatfs.c implement the controller for more devices inside USB_HostMsdEvent, for example, in the kUSB_HostEventAttach event you find:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;g_MsdFatfsInstance&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;deviceState &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; kStatus_DEV_Idle&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="comment token"&gt;/* the interface is supported by the application */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;g_MsdFatfsInstance&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;deviceHandle &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; deviceHandle&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;g_MsdFatfsInstance&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;interfaceHandle &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; interface&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;g_MsdFatfsInstance&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;configHandle &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; configurationHandle&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; kStatus_USB_Success&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;In this case you will have to implement a count of devices to use different handlers. This instance is also used in kUSB_HostEventEnumerationDone and in kUSB_HostEventDetach events&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information could help you.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Jun 2017 23:57:08 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2017-06-29T23:57:08Z</dc:date>
    <item>
      <title>Mount 2 MSD with FATfs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mount-2-MSD-with-FATfs/m-p/687133#M42299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on USB stack(TWR_K22F120MA). FAT demo works pretty good with single pendrive. But when i connect hub and connect two pen drives. i am not able to mount 2 pen drives to 2 different drives. and i believe code also does not support for multi-drive implementation.&lt;/P&gt;&lt;P&gt;So if somebody please guide me or give me code snippets to work for multi-drive implementation, it will be a great help.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Aniket&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jun 2017 17:53:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mount-2-MSD-with-FATfs/m-p/687133#M42299</guid>
      <dc:creator>aniketmarkande</dc:creator>
      <dc:date>2017-06-14T17:53:08Z</dc:date>
    </item>
    <item>
      <title>Re: Mount 2 MSD with FATfs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mount-2-MSD-with-FATfs/m-p/687134#M42300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Aniket Markande&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, if you are using the latest USB stack (the one that comes with SDK2.x), it already support HUB drivers. You can find in usb_host_config.h file a macro definitions as #define USB_HOST_CONFIG_HUB (1U), this will enable Host HUB class driver is enable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regardless of this, the given example doesn't implement the support for more MSD, but you can add it to it:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. You have to add a new mass storage device instance, the example uses the g_MsdFatfsInstance global variable for the instance, so you could add a g_MsdFatfsInstance_2.&lt;/P&gt;&lt;P&gt;2. Inside app.c you can see that this instance is used to create the task with USB_HostMsdTask(&amp;amp;g_MsdFatfsInstance); (this variable is declared here as extern because we actually used in host_msd_fatfs.c).&lt;/P&gt;&lt;P&gt;3. In host_msd_fatfs.c implement the controller for more devices inside USB_HostMsdEvent, for example, in the kUSB_HostEventAttach event you find:&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;g_MsdFatfsInstance&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;deviceState &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; kStatus_DEV_Idle&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="comment token"&gt;/* the interface is supported by the application */&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;g_MsdFatfsInstance&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;deviceHandle &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; deviceHandle&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;g_MsdFatfsInstance&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;interfaceHandle &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; interface&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;g_MsdFatfsInstance&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;configHandle &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; configurationHandle&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt; kStatus_USB_Success&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;In this case you will have to implement a count of devices to use different handlers. This instance is also used in kUSB_HostEventEnumerationDone and in kUSB_HostEventDetach events&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information could help you.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2017 23:57:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mount-2-MSD-with-FATfs/m-p/687134#M42300</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-06-29T23:57:08Z</dc:date>
    </item>
    <item>
      <title>Re: Mount 2 MSD with FATfs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mount-2-MSD-with-FATfs/m-p/687135#M42301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply and i was able to run two mass storage devices :smileyhappy:&lt;/P&gt;&lt;P&gt;Now i have one more device connected to hub which is speaker and the problem is "USB_HostEvent()" is common callback for attach/detach. Then how to differentiate which device has been connected?&lt;/P&gt;&lt;P&gt;I tried this way, but it causes problem.&lt;/P&gt;&lt;P&gt;STATIC usb_status_t USB_HostEvent(usb_device_handle deviceHandle,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; usb_host_configuration_handle configurationHandle,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t eventCode)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; usb_status_t status = kStatus_USB_Success;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; switch (eventCode)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; case kUSB_HostEventAttach:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; case kUSB_HostEventEnumerationDone:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; case kUSB_HostEventDetach:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;status = USB_HostMsdEvent(deviceHandle, configurationHandle, eventCode);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;status = USB_HostAudioEvent(deviceHandle, configurationHandle, eventCode);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; case kUSB_HostEventNotSupported:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; usb_echo("Unsupported Device\r\n");&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; default:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return status;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Sep 2017 07:27:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mount-2-MSD-with-FATfs/m-p/687135#M42301</guid>
      <dc:creator>aniketmarkande</dc:creator>
      <dc:date>2017-09-29T07:27:15Z</dc:date>
    </item>
    <item>
      <title>Re: Mount 2 MSD with FATfs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mount-2-MSD-with-FATfs/m-p/687136#M42302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i have mounted 1 MSD on 0: and another on 1: , is this correct (as a two physical drives)?&lt;/P&gt;&lt;P&gt;Also when i am trying to change drive using f_chdrive(), its changing the drive variable CurrVol in code. But when i perform any operation it is performed on last drive which i have mounted.&lt;/P&gt;&lt;P&gt;please guide me on how to mount two MSD devices and access them simultaneously using FATfs.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Oct 2017 09:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Mount-2-MSD-with-FATfs/m-p/687136#M42302</guid>
      <dc:creator>aniketmarkande</dc:creator>
      <dc:date>2017-10-06T09:28:48Z</dc:date>
    </item>
  </channel>
</rss>