<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 [TWR-K65 + TWR-Ser] Using USBHS and USBFS</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K65-TWR-Ser-Using-USBHS-and-USBFS/m-p/686550#M42255</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a TWR-K65 board where I can run the usb-device-cdc-vcom-example using the USB-HS port. Using the TWR-K65 standalone this works!&lt;/P&gt;&lt;P&gt;But as soon as I connect the TWR-SER to the tower stack, it stops working.&lt;/P&gt;&lt;P&gt;It seems that the K65 sees the USB bus permanently in reset state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My goal is to use both USB (USBHS and USBFS). The USBHS over the USB connector on the TWR-K65 as a device and the USBFS over the USB connector on the TWR-SER as a host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas whats wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Jul 2017 08:32:32 GMT</pubDate>
    <dc:creator>baltech</dc:creator>
    <dc:date>2017-07-28T08:32:32Z</dc:date>
    <item>
      <title>[TWR-K65 + TWR-Ser] Using USBHS and USBFS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K65-TWR-Ser-Using-USBHS-and-USBFS/m-p/686550#M42255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a TWR-K65 board where I can run the usb-device-cdc-vcom-example using the USB-HS port. Using the TWR-K65 standalone this works!&lt;/P&gt;&lt;P&gt;But as soon as I connect the TWR-SER to the tower stack, it stops working.&lt;/P&gt;&lt;P&gt;It seems that the K65 sees the USB bus permanently in reset state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My goal is to use both USB (USBHS and USBFS). The USBHS over the USB connector on the TWR-K65 as a device and the USBFS over the USB connector on the TWR-SER as a host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas whats wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2017 08:32:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K65-TWR-Ser-Using-USBHS-and-USBFS/m-p/686550#M42255</guid>
      <dc:creator>baltech</dc:creator>
      <dc:date>2017-07-28T08:32:32Z</dc:date>
    </item>
    <item>
      <title>Re: [TWR-K65 + TWR-Ser] Using USBHS and USBFS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K65-TWR-Ser-Using-USBHS-and-USBFS/m-p/686551#M42256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The TWR-K65F180M board user guide shows below info:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6357i15CBADE3B5D7B056/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So, we need to use USB HS with on-board Micro USB connector J15 and USB FS with TWR-SER board J14.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do a test with MCUXpresso SDK V2.2 for TWR-K65F180M board with [usb_keyboard2mouse] demo, which using FS USB as USB host and HS USB as USB device.&lt;/P&gt;&lt;P&gt;..\SDK_2.2_TWR-K65F180M\boards\twrk65f180m\usb_examples\usb_keyboard2mouse&lt;/P&gt;&lt;P&gt;That demo works as expected.&lt;/P&gt;&lt;P&gt;Below is my test hardware platform:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/6432iD2DEFC0EB1D33491/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I also attached the test result with attached video file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check you are using TWR-SER board as USB FS connector. And the TWR-K65F180M R189 and R190 using 0ohm resistor at side A, not side B.&lt;/P&gt;&lt;P&gt;If K65 FS USB as USB host, the TWR-SER board jumper setting J10 1-2, J16 1-2.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 06:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K65-TWR-Ser-Using-USBHS-and-USBFS/m-p/686551#M42256</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-08-01T06:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: [TWR-K65 + TWR-Ser] Using USBHS and USBFS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K65-TWR-Ser-Using-USBHS-and-USBFS/m-p/686552#M42257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thanks for your detailed answer!&lt;/P&gt;&lt;P&gt;It was not working with your setup.&lt;/P&gt;&lt;P&gt;But I figured out I have to remove on of the both jumper at J23 on my TWR-K65. Now it is working as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Aug 2017 09:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K65-TWR-Ser-Using-USBHS-and-USBFS/m-p/686552#M42257</guid>
      <dc:creator>baltech</dc:creator>
      <dc:date>2017-08-01T09:18:19Z</dc:date>
    </item>
  </channel>
</rss>