<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Issue with CAN(Tx) for KEAZ128, SDK platform in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Issue-with-CAN-Tx-for-KEAZ128-SDK-platform/m-p/685902#M42211</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am using one of the examples i found on this community. I am using FRDM- KEAZ128 development board and want to send CAN data from the board( TX). Moreover i am using SDK instead of using code warrior.( i believe i took this code from one of the posts that mentions the problem with using NVIC.h file for SDK platform, and then someone uploaded a code compatible with SDK) I can compile the code without any issues, however, when i put it in debug mode, i can see a path error. I tried updating the path from source lookup path preferences, but i am still getting a path issue which throws an error : No source available for init CAN() at 0 x 498.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am new to this platform and not sure where i am going wrong. The code is attached with this post.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Can someone please help me understanding the issue.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337684"&gt;KEAZ128_Community_MSCAN.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jun 2017 13:19:09 GMT</pubDate>
    <dc:creator>aveshshah</dc:creator>
    <dc:date>2017-06-13T13:19:09Z</dc:date>
    <item>
      <title>Issue with CAN(Tx) for KEAZ128, SDK platform</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Issue-with-CAN-Tx-for-KEAZ128-SDK-platform/m-p/685902#M42211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am using one of the examples i found on this community. I am using FRDM- KEAZ128 development board and want to send CAN data from the board( TX). Moreover i am using SDK instead of using code warrior.( i believe i took this code from one of the posts that mentions the problem with using NVIC.h file for SDK platform, and then someone uploaded a code compatible with SDK) I can compile the code without any issues, however, when i put it in debug mode, i can see a path error. I tried updating the path from source lookup path preferences, but i am still getting a path issue which throws an error : No source available for init CAN() at 0 x 498.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;I am new to this platform and not sure where i am going wrong. The code is attached with this post.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Can someone please help me understanding the issue.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337684"&gt;KEAZ128_Community_MSCAN.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jun 2017 13:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Issue-with-CAN-Tx-for-KEAZ128-SDK-platform/m-p/685902#M42211</guid>
      <dc:creator>aveshshah</dc:creator>
      <dc:date>2017-06-13T13:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with CAN(Tx) for KEAZ128, SDK platform</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Issue-with-CAN-Tx-for-KEAZ128-SDK-platform/m-p/685903#M42212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Avesh,&lt;/P&gt;&lt;P&gt;I think your project lacks of some files, I tried to compile it, there was not makefile, so I failed to compile the project.&lt;/P&gt;&lt;P&gt;i suggest you create a new project based on KDS tools, copy the source code to the new project, recompile.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 07:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Issue-with-CAN-Tx-for-KEAZ128-SDK-platform/m-p/685903#M42212</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-06-15T07:26:14Z</dc:date>
    </item>
  </channel>
</rss>