<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Reply for Project Creation</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reply-for-Project-Creation/m-p/684355#M42130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Snehal:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Installing an SDK, please first download the SDK package, then install this into MCUXpresso IDE. The easiest way to do this is to switch to the "Installed SDKs" view within the MCUXpresso IDE console view. simply open a Windows Explore / filter onto the directory containing the SDK packages, then select the ZIP files and drag them into the "Intalled SDKs" view.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19780i1BB957B7F0C7E47F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 May 2017 06:34:33 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2017-05-23T06:34:33Z</dc:date>
    <item>
      <title>Reply for Project Creation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reply-for-Project-Creation/m-p/684354#M42129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;I have used SDK builder from mcuexpresso.nxp.com. I have downloaded the received zip file from that&amp;nbsp;&lt;/P&gt;&lt;P&gt;SDK Builder but when I am trying to add it from&lt;/P&gt;&lt;P&gt;Help -&amp;gt; Install New Software-&amp;gt; Add -&amp;gt;Archieve&lt;/P&gt;&lt;P&gt;It is giving me following error&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20004iED4E4914C2DB3407/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 May 2017 07:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reply-for-Project-Creation/m-p/684354#M42129</guid>
      <dc:creator>snehalnigudkar</dc:creator>
      <dc:date>2017-05-18T07:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: Reply for Project Creation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reply-for-Project-Creation/m-p/684355#M42130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Snehal:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Installing an SDK, please first download the SDK package, then install this into MCUXpresso IDE. The easiest way to do this is to switch to the "Installed SDKs" view within the MCUXpresso IDE console view. simply open a Windows Explore / filter onto the directory containing the SDK packages, then select the ZIP files and drag them into the "Intalled SDKs" view.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19780i1BB957B7F0C7E47F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 May 2017 06:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Reply-for-Project-Creation/m-p/684355#M42130</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2017-05-23T06:34:33Z</dc:date>
    </item>
  </channel>
</rss>