<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Where has the FPU gone???</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683451#M42085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A second prototype has a chip from the same batch on it and it works normally (has FPU, USB0, FlexCAN etc.) and returns the expected ID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any possible explanation for the first one's behavior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Aug 2017 01:32:08 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2017-08-09T01:32:08Z</dc:date>
    <item>
      <title>Where has the FPU gone???</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683446#M42080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone explain this?&lt;/P&gt;&lt;P&gt;- I have the FRDM-K66F board with the K66FN2M on it and a simple program that operates as normal.&lt;BR /&gt;- Then I have a new HW with a K66FX1M on it and am expecting the same code to run on it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The new HW however hard faults when the FPU initialisation takes place (before any clock initialisation).&lt;/P&gt;&lt;P&gt;When I look at the default FPU system registers (after reset and before doing anything else) on the FRDM-K66F I see this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27874i2B8A56731F62205E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I look at the registers on the new HW they are all at 0x00000000 and any code access to the registers is met with the hard fault.&lt;/P&gt;&lt;P&gt;So the question is, what can cause the FPU not to operate (normally) ???? I am expecting it to be to do with a HW connection (maybe a missing power pin?) since the prototype is hand built but there must be a logical explanation to aid in tracking down whatever it is.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Power supply is otherwise 3.3V exactly.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jul 2017 22:57:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683446#M42080</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-07-25T22:57:46Z</dc:date>
    </item>
    <item>
      <title>Re: Where has the FPU gone???</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683447#M42081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Curiouser and curioser.....&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The ID on the FRDM-K66FN2M0 part is 0x660083ca, which means K66, rev. 8, 144-pins&lt;/P&gt;&lt;P&gt;The ID on the K66FX1M0 is 0x160083ff, which means K16, rev. 8 with reserved family ID and reserved&amp;nbsp; pin count identification (there is no K16 that I can find).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I configure the compiler to use SW FPU rather than the internal FPU the code runs on the K66FX1M0. However when I try to use the FS USB on it it hard faults on an USB access.&lt;BR /&gt;The reason being that, according to the SIM_SCGCx registers (which if one writes 0xffffffff to the bits that stick show the modules available) there is no &lt;STRONG&gt;USB0&lt;/STRONG&gt; in the chip. Also it shows no &lt;STRONG&gt;SDHC&lt;/STRONG&gt; or &lt;STRONG&gt;FlexCAN1&lt;/STRONG&gt;. No &lt;STRONG&gt;USBDCD&lt;/STRONG&gt;, no &lt;STRONG&gt;RNGA&lt;/STRONG&gt;, no &lt;STRONG&gt;FlexCAN0&lt;/STRONG&gt;, no &lt;STRONG&gt;Ethernet&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the package it is marked MK66FX1M0VLQ18, Mask 0N65N, batch OAK1712C - and it was originally delivered with the KBOOT loader programmed in Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;Is it possible that this is some form of dud (re-packaged reject?) that has been delivered?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 00:41:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683447#M42081</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-07-26T00:41:31Z</dc:date>
    </item>
    <item>
      <title>Re: Where has the FPU gone???</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683448#M42082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you let us know which channel do you get that chip(MK66FX1M0VLQ18) from? NXP distributor or e-trader?&lt;/P&gt;&lt;P&gt;How many chips(MK66FX1M0VLQ18) do you have? If all with the same behavior?&lt;/P&gt;&lt;P&gt;The normal MK66FX1M0VLQ18 chip should provides SDHC, FlexCAN(2), USBDCD,&amp;nbsp; Ethernet, RNGA, USB0 also.&lt;/P&gt;&lt;P&gt;I checked the MK66FX1M0VLQ18 sample in stock, could you use&lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/kinetis-cortex-m-mcus/k-series-performance-m4/k6x-ethernet/kinetis-k66-180-mhz-dual-high-speed-full-speed-usbs-2mb-flash-microcontrollers-mcus-based-on-arm-cortex-m4-core:K66_180?tab=Buy_Parametric_Tab"&gt; this link&lt;/A&gt; to apply for that chip samples?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27102iECD19A0A257D9039/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 05:24:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683448#M42082</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-07-26T05:24:06Z</dc:date>
    </item>
    <item>
      <title>Re: Where has the FPU gone???</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683449#M42083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The chip was ordered here:&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.mouser.it%2FSearch%2FProductDetail.aspx%3FR%3DMK66FX1M0VLQ18virtualkey55700000virtualkey841-MK66FX1M0VLQ18" rel="nofollow" target="_blank"&gt;http://www.mouser.it/Search/ProductDetail.aspx?R=MK66FX1M0VLQ18virtualkey55700000virtualkey841-MK66FX1M0VLQ18&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is only one prototype available at the moment which I received from my client, but I have asked whether additional ones may be possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 12:27:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683449#M42083</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-07-26T12:27:20Z</dc:date>
    </item>
    <item>
      <title>Re: Where has the FPU gone???</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683450#M42084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let us know if the other one still with the same issue. Thank you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 00:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683450#M42084</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-07-27T00:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: Where has the FPU gone???</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683451#M42085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A second prototype has a chip from the same batch on it and it works normally (has FPU, USB0, FlexCAN etc.) and returns the expected ID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any possible explanation for the first one's behavior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 01:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683451#M42085</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-08-09T01:32:08Z</dc:date>
    </item>
    <item>
      <title>Re: Where has the FPU gone???</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683452#M42086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the first one, I am checking with Kinetis product team.&lt;/P&gt;&lt;P&gt;I will let you know the feedback later. Thanks.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Aug 2017 02:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Where-has-the-FPU-gone/m-p/683452#M42086</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-08-10T02:02:46Z</dc:date>
    </item>
  </channel>
</rss>