<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: can i program MKW41Z512 without sda controller?or direct  using rs232</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/can-i-program-MKW41Z512-without-sda-controller-or-direct-using/m-p/683129#M42064</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can use a J-LINK to program the microcontroller, as well as the OpenSDA. If you have a bootloader you could also program it with UART or SPI just as it is done with the Kinetis Wireless Host Application Programming Interface (Host API).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Kinetis Wireless Host Application Programming Interface (Host API)&amp;nbsp;implements the Framework Serial Connectivity Interface (FSCI) on a peripheral port such as UART, USB, and SPI; the documentation and the stack it’s located in the SDK of the FRDM-KW41Z that you can download from&amp;nbsp;&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;MCUXpresso&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 May 2017 14:26:54 GMT</pubDate>
    <dc:creator>stephanie_m</dc:creator>
    <dc:date>2017-05-26T14:26:54Z</dc:date>
    <item>
      <title>can i program MKW41Z512 without sda controller?or direct  using rs232</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/can-i-program-MKW41Z512-without-sda-controller-or-direct-using/m-p/683128#M42063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am sheshnath chauhan and i want to know about MKW41Z512 controller programming option except sda.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/space/2019"&gt;Kinetis Microcontrollers&lt;/A&gt;‌&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/dhaval"&gt;dhaval&lt;/A&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/khumphri"&gt;khumphri&lt;/A&gt;&lt;A href="https://community.nxp.com/community/about"&gt;https://community.nxp.com/community/about&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 07:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/can-i-program-MKW41Z512-without-sda-controller-or-direct-using/m-p/683128#M42063</guid>
      <dc:creator>sheshnathchauha</dc:creator>
      <dc:date>2017-05-17T07:23:46Z</dc:date>
    </item>
    <item>
      <title>Re: can i program MKW41Z512 without sda controller?or direct  using rs232</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/can-i-program-MKW41Z512-without-sda-controller-or-direct-using/m-p/683129#M42064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can use a J-LINK to program the microcontroller, as well as the OpenSDA. If you have a bootloader you could also program it with UART or SPI just as it is done with the Kinetis Wireless Host Application Programming Interface (Host API).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Kinetis Wireless Host Application Programming Interface (Host API)&amp;nbsp;implements the Framework Serial Connectivity Interface (FSCI) on a peripheral port such as UART, USB, and SPI; the documentation and the stack it’s located in the SDK of the FRDM-KW41Z that you can download from&amp;nbsp;&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;MCUXpresso&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 May 2017 14:26:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/can-i-program-MKW41Z512-without-sda-controller-or-direct-using/m-p/683129#M42064</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2017-05-26T14:26:54Z</dc:date>
    </item>
    <item>
      <title>Re: can i program MKW41Z512 without sda controller?or direct  using rs232</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/can-i-program-MKW41Z512-without-sda-controller-or-direct-using/m-p/683130#M42065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I don't have boot loader . Could you please tell me about the bootloader&lt;/P&gt;&lt;P&gt;and how can get it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On 26-May-2017 7:57 PM, "estephania_martinez" &amp;lt;admin@community.nxp.com&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 May 2017 12:43:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/can-i-program-MKW41Z512-without-sda-controller-or-direct-using/m-p/683130#M42065</guid>
      <dc:creator>sheshnathchauha</dc:creator>
      <dc:date>2017-05-31T12:43:42Z</dc:date>
    </item>
    <item>
      <title>Re: can i program MKW41Z512 without sda controller?or direct  using rs232</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/can-i-program-MKW41Z512-without-sda-controller-or-direct-using/m-p/683131#M42066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find more information about the bootloader in the Kinetis Thread Stack and FSCI Bootloader Quick Start Guide.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find this document in the SDK release I mentioned in the first reply under the following path:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;download path&amp;gt;\SDK_2.2_FRDM-KW41Z\docs\wireless\Thread\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if you have any other doubt&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 May 2017 23:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/can-i-program-MKW41Z512-without-sda-controller-or-direct-using/m-p/683131#M42066</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2017-05-31T23:12:19Z</dc:date>
    </item>
  </channel>
</rss>