<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KV46 : How to get a system/core clock @ 100MHz with 8 MHz crystal</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-How-to-get-a-system-core-clock-100MHz-with-8-MHz-crystal/m-p/681921#M41996</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for pointing this part of the datasheet out. Answer is clear.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 May 2017 12:33:47 GMT</pubDate>
    <dc:creator>frq04646</dc:creator>
    <dc:date>2017-05-17T12:33:47Z</dc:date>
    <item>
      <title>KV46 : How to get a system/core clock @ 100MHz with 8 MHz crystal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-How-to-get-a-system-core-clock-100MHz-with-8-MHz-crystal/m-p/681919#M41994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using board HVP-KV46F150M, with KV46 on it.&lt;/P&gt;&lt;P&gt;KV46 is clocked with external crystal @ 8 MHz, with load capacitors @ 10pF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to set up system &amp;amp; core clocks to 100 MHz, which is the maximum in RUN mode, according to datasheet.&lt;/P&gt;&lt;P&gt;However, I can't find a configuration matching this requirement when using MCUXpresso Clock Tool.&lt;/P&gt;&lt;P&gt;The reason is that the PLL output frequency must be in range 220 MHz - 480 MHz, and the only way I found to get 100MHz on system/core clock is to have PLL output @ 200 MHz (see attached capture)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea ?&lt;/P&gt;&lt;P&gt;Thanks !&lt;/P&gt;&lt;P&gt;Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 14:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-How-to-get-a-system-core-clock-100MHz-with-8-MHz-crystal/m-p/681919#M41994</guid>
      <dc:creator>frq04646</dc:creator>
      <dc:date>2017-05-16T14:23:45Z</dc:date>
    </item>
    <item>
      <title>Re: KV46 : How to get a system/core clock @ 100MHz with 8 MHz crystal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-How-to-get-a-system-core-clock-100MHz-with-8-MHz-crystal/m-p/681920#M41995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pierre,&lt;/P&gt;&lt;P&gt;- It seems if the external crystal is 8Mhz, the PEE mode can not generate core clock with 100MHZ.&lt;/P&gt;&lt;P&gt;From the datasheet we can see the PLL output range is 110MHZ - 240MHZ,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20677i3BB3790EEBBF65DA/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;so the range of PLL on Clock configure tool is 220 - 480 , it can't choose 200MHZ.&lt;/P&gt;&lt;P&gt;- You can increase the external crystal, for example 16MHZ:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20716i49BB3A77DFA51C8E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 10:11:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-How-to-get-a-system-core-clock-100MHz-with-8-MHz-crystal/m-p/681920#M41995</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-05-17T10:11:27Z</dc:date>
    </item>
    <item>
      <title>Re: KV46 : How to get a system/core clock @ 100MHz with 8 MHz crystal</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-How-to-get-a-system-core-clock-100MHz-with-8-MHz-crystal/m-p/681921#M41996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for pointing this part of the datasheet out. Answer is clear.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Pierre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 12:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-How-to-get-a-system-core-clock-100MHz-with-8-MHz-crystal/m-p/681921#M41996</guid>
      <dc:creator>frq04646</dc:creator>
      <dc:date>2017-05-17T12:33:47Z</dc:date>
    </item>
  </channel>
</rss>