<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Flexbus secondary wait states functionality and configuration</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-secondary-wait-states-functionality-and-configuration/m-p/681145#M41938</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The secondary wait states only applied for burst operation.&lt;/P&gt;&lt;P&gt;In fact, the MCUXpresso SDK V2.2.0 software Flexbus driver doesn't provide full features of the Flexbus module.&lt;/P&gt;&lt;P&gt;Customer can add related secondary wait states setting function in application code.&lt;/P&gt;&lt;P&gt;Sorry for that may bring any inconvenience to you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jul 2017 04:58:55 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2017-07-26T04:58:55Z</dc:date>
    <item>
      <title>Flexbus secondary wait states functionality and configuration</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-secondary-wait-states-functionality-and-configuration/m-p/681144#M41937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First, do secondary wait states only apply to burst operations, or can they be treated as an extension of the primary wait states for single byte accesses?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regardless, there doesn't appear to be a way to set the secondary wait state value. The&amp;nbsp;_flexbus_config structure has a boolean for enabling the secondary wait states, but the is no field for the number of wait states. Not surprisingly, there is no code in FLEXBUS_Init() to set the appropriate bits in the CSCR register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is using MCUXpresso 10.0.2 and an SDK 2.2.0 built for the TWR-K64F120M.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 15:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-secondary-wait-states-functionality-and-configuration/m-p/681144#M41937</guid>
      <dc:creator>yorknh</dc:creator>
      <dc:date>2017-07-24T15:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: Flexbus secondary wait states functionality and configuration</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-secondary-wait-states-functionality-and-configuration/m-p/681145#M41938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The secondary wait states only applied for burst operation.&lt;/P&gt;&lt;P&gt;In fact, the MCUXpresso SDK V2.2.0 software Flexbus driver doesn't provide full features of the Flexbus module.&lt;/P&gt;&lt;P&gt;Customer can add related secondary wait states setting function in application code.&lt;/P&gt;&lt;P&gt;Sorry for that may bring any inconvenience to you.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 04:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flexbus-secondary-wait-states-functionality-and-configuration/m-p/681145#M41938</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-07-26T04:58:55Z</dc:date>
    </item>
  </channel>
</rss>