<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Configure UART to wake up MK10DN64 in VLPS mode in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Configure-UART-to-wake-up-MK10DN64-in-VLPS-mode/m-p/680764#M41900</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use MK10DN64 as TSI can use all channels to wake up MCU from VLPS low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But i want to use both TSI all channels and UART to wake up the MCU from low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For this how can i configure MCU in VLPS mode (using PE) and use UART to wake up the MCU and which UART do i need to configure as there no specific low power UARTs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jul 2017 10:39:48 GMT</pubDate>
    <dc:creator>karthikbandi</dc:creator>
    <dc:date>2017-07-24T10:39:48Z</dc:date>
    <item>
      <title>Configure UART to wake up MK10DN64 in VLPS mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Configure-UART-to-wake-up-MK10DN64-in-VLPS-mode/m-p/680764#M41900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use MK10DN64 as TSI can use all channels to wake up MCU from VLPS low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But i want to use both TSI all channels and UART to wake up the MCU from low power mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For this how can i configure MCU in VLPS mode (using PE) and use UART to wake up the MCU and which UART do i need to configure as there no specific low power UARTs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 10:39:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Configure-UART-to-wake-up-MK10DN64-in-VLPS-mode/m-p/680764#M41900</guid>
      <dc:creator>karthikbandi</dc:creator>
      <dc:date>2017-07-24T10:39:48Z</dc:date>
    </item>
  </channel>
</rss>