<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: flexbus sleep mode current</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexbus-sleep-mode-current/m-p/680643#M41895</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K65 datasheet list power consumption is only the K65 chip power consumption, not the board power consumption.&lt;/P&gt;&lt;P&gt;Please refer TWR-K65F180M board schematics, the power consumption measure point at jumper J1.&lt;/P&gt;&lt;P&gt;If it is possible, could you please provide your board schematics here?&lt;/P&gt;&lt;P&gt;For NXP community is a public forum, customer could refer below document to create a service case to post your board schematics.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-wiki-small" data-containerid="2001" data-containertype="14" data-objectid="329745" data-objecttype="102" href="https://community.nxp.com/docs/DOC-329745"&gt;https://community.nxp.com/docs/DOC-329745&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Jul 2017 05:33:20 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2017-07-05T05:33:20Z</dc:date>
    <item>
      <title>flexbus sleep mode current</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexbus-sleep-mode-current/m-p/680642#M41894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a K65 on a target board with external NOR Flash and an LCD display connected to the flexbus. For sleep mode I am putting the processor&amp;nbsp;into the LLS mode. What I experience is varying levels of sleep mode current - from a low of 0.1 mA up to 1.1 mA. I have traced this discrepancy to the flexbus signals. By disabling the data and address lines (setting the pin mux control in the Portx_PCRn registers to 0 upon entering sleep) I have almost completely eliminated the discrepancy for all 40 prototype boards tested. Has anyone else experienced this type of behavior in sleep mode? &amp;nbsp;Is there something in the design or layout that I should be looking at as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Elizabeth&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 17:16:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexbus-sleep-mode-current/m-p/680642#M41894</guid>
      <dc:creator>ERussell</dc:creator>
      <dc:date>2017-06-30T17:16:08Z</dc:date>
    </item>
    <item>
      <title>Re: flexbus sleep mode current</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexbus-sleep-mode-current/m-p/680643#M41895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K65 datasheet list power consumption is only the K65 chip power consumption, not the board power consumption.&lt;/P&gt;&lt;P&gt;Please refer TWR-K65F180M board schematics, the power consumption measure point at jumper J1.&lt;/P&gt;&lt;P&gt;If it is possible, could you please provide your board schematics here?&lt;/P&gt;&lt;P&gt;For NXP community is a public forum, customer could refer below document to create a service case to post your board schematics.&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-wiki-small" data-containerid="2001" data-containertype="14" data-objectid="329745" data-objecttype="102" href="https://community.nxp.com/docs/DOC-329745"&gt;https://community.nxp.com/docs/DOC-329745&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2017 05:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/flexbus-sleep-mode-current/m-p/680643#M41895</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2017-07-05T05:33:20Z</dc:date>
    </item>
  </channel>
</rss>